Skip to main content
ffwali
Visitor II
September 29, 2022
Question

How to add and switch between multiple eSIM profiles in ST4SIM200?

  • September 29, 2022
  • 7 replies
  • 2751 views

I have B-L462E-CELL1 development board with ST4SIM200M IC. this board came pre-provisioned with the Truphone profile but I didn't find any way to add a new profile. According to the datasheet eSIm chip supports up to 7 profiles but How can we add and switch between different profiles?

    This topic has been closed for replies.

    7 replies

    Visitor II
    January 21, 2025

    I also have same question i bouth st4sim-200 ic and want add more sim profiles. But dont know which tool to use for that action.

    Agostino VANORE
    ST Employee
    January 21, 2025

    Hi, the ST4SIM-200 is configured with 1GLOBAL (former Truphone) connectivity, and 1GLOBAL is also configured as Subscription Management platform (SM-SR), able to manage remotely the profile on the eSIM.

    According the GSMA SGP.02 specification/architecture, the new profile to be downloaded, shall be available on the SM-DP of the operator and the SM-DP integrated with the SM-SR managing the eSIM.

    That said, the profile download shall be managed through SM-SR and in that case referring to 1GLOBAL.

    The drawback/limitation of this architecture is that the SM-DP of the operator you want to download is not available on 1GLOBAL SM-SR.

    Andrew Neil
    Super User
    January 21, 2025

    @Agostino VANORE wrote:

    It's not possible to program. The only way is through 1GLOBAL partner.


    Indeed.

    @Kobra1991 @ffwali remember that the 'S' in "SIM" stands for "Subscriber" - ie, the one who pays for the service.

    The SIM credentials are all about ensuring that the service provider gets paid - so they're not going to allow anyone to just go randomly creating SIMs!

     

    #eSIM #SIMProfile

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.