cancel
Showing results for 
Search instead for 
Did you mean: 

Good morning, is there any specific PC software application that can be used with SensorTile kit instead of the Mobile application?

stephane hoareau
Associate II
Posted on November 06, 2017 at 11:15

Good morning, is there any specific PC software application that can be used with SensorTile kit instead of the Mobile application?

My point is to have the same features that can be performed form my labtop instead of the mobile.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Antonio Vilei
ST Employee
Posted on November 08, 2017 at 18:29

Hi Stéphane,

as the SensorTile is mainly thought for wearable applications, the mobile app (communicating via Bluetooth Low Energy) is the preferred way to test its features. There is no equivalent PC application that is able to test all the features of the SensorTile.

Based on your needs, you could use USB to transmit data using a virtual serial port (CDC class) or to stream audio using the USB Audio class.

Best regards,

Antonio

Posted on November 09, 2017 at 12:53

If your laptop has BLE, it could use that to communicate with the Tile in exactly the same way that the app does.

AIUI, you need Win10 for native BLE support.

Or maybe you could find a BLE 'dongle' with a suitable API ...

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.