2024-10-29 5:42 AM
Hi,
here is a post for wireless community (Sub-1Ghz solutions) to answer many frequently asked questions and good practices using ST S2-LP transceiver.
please find attached document to get additional information on this perfect Radio chipset.
Thanks
Philippe
2026-04-18 6:09 AM
@Philippe SIMONNET Can you link this document to the product's page?
2026-04-23 6:56 AM
Hi Cezar,
wiki page is done, should be quickly available for community (under approval)
Thanks
Philippe
2026-04-23 7:10 AM
@Philippe SIMONNET maybe pin this thread ?
2026-05-20 6:30 AM
Dear Mr. Simonnet,
We are currently using the newer STM32WL33 (M0+MRSubG) for a receiver-only application, and given that the transmitter is continuously transmitting (inserting stuffing bytes between well-formatted packets), we had to adapt the HAL code to a good extent.
I found this document and read with much attention the S2-LP recommendations.
Are this document still applicable (and to which extent) to the STM32WL33?
In particular, STM32WL33 has the "AFC3" register, which has no direct equivalent in S2-LP.
Thanks in advance,
Renzo Posega
2026-05-21 12:04 AM
Hi Renzo,
S2-LP recommendations are more or less applicable to WL3x radio, even if :
- WL3x is RF SoC / S2-LP transceiver
- there are WL3x radio improvements, so register changes happen
regarding AFC, I can give you recommendations if you tell me Radio configuration you have to use (modulation, packet mode/direct mode, ...)
or you can also rich me entering support request here Online Support
(please mention my name, to route ticket to me as fast as possible)
thanks
Philippe
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.