Skip to main content
Associate
July 28, 2025
Question

VL53L1X_CheckForDataReady returns VL53L1_ERROR_CONTROL_INTERFACE

I was trying to implement VL53L1 TOF sensor on VL53L1-SATEL breakout board with STM Nucleo C071RB development board using STSW IMG009 VL53L1X Ultra Lite Driver.

By following the example after init, boot, setup and startRanging I called VL53L1X_CheckForDataReady(), which always returned error -13 - VL53L1_ERROR_CONTROL_INTERFACE . After extensive checking of I2C interface I figured out that this error occurs when VL53L1X_GetInterruptPolarity() is called (within checkForDataReady or independently) when ranging is active. If ranging is stopped, GetInterruptPolarity() works just fine.

My solution was to write my own library of required functions that further rely on VL53L1X_api. Before start ranging, I read the Interrupt Polarity, store it locally and then use modified checkForDataReady() function, which uses stored InterruptPolarity to check if new data is available.

Has anyone else noticed such behaviour?

This also connects to topics:
https://community.st.com/t5/imaging-sensors/vl53l1x-interrupt-not-working-no-measurements/td-p/650785

https://community.st.com/t5/imaging-sensors/vl53l1x-vl53l1-error-control-interface-when-vl53l1/td-p/386039 

Best regards

This topic has been closed for replies.

1 reply

Zhiyuan.Han
ST Technical Moderator
July 29, 2025

Hi

When sensor is raging, if you try to read out the value, it could return error.You need to read out the data after data is ready. 

From your description, you have modified some of the API to build you own library. can you try run the code with the unchanged API?

Please share your code and log for further debug. 

 

Br

Zhiyuan.Han

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.