Skip to main content
Will_Robertson
Associate III
December 29, 2024
Solved

Drivers for ST BrightSense Image Sensors for STM32N6 Series μCs and STM32MP2 Series SoCs

  • December 29, 2024
  • 10 replies
  • 1961 views

Hi,

I was wondering if there were plans to make drivers for the ST BrightSense image sensors available for the ST STM32N6 Series μCs (these could be bare metal, FreeRTOS, ThreadX or Zephyr drivers) or for ST STM32MP2 Series SoMs (in the form of libcamera drivers)?

I heard that drivers for the VD66GY image sensor are planned for the STM32N6 Series μCs but I wasn't sure about the other BrightSense image sensors.

Providing drivers for the ST BrightSense image sensors for the STM32N6 Series μCs and STM32MP2 Series SoCs would allow ST customers to fully leverage the enormous power of both ST image sensors and the leading ISP and AI capabilities of STM32N6 and STM32MP2 while developing a solution entirely within the ST ecosystem. Having drivers provided by ST instead of coding our own drivers would enormously speed route to market and reduce risk.

Thank you very much for your help.

Will

This topic has been closed for replies.
Best answer by CyrilTechPro

Hello Will, 

 

First of all, Happy New Year, 

 

Today the VD66GY and VD55G1 are released regarding STM32N6 We work to add ASAP the other sensor and provide code example. It is one of the priority.

 

We work also to provide libcamera + ST driver on STlinux it will be in a second time after STM32N6 

 

Regards 

Cyril Liotard 

 

 

10 replies

CyrilTechProBest answer
ST Employee
January 13, 2025

Hello Will, 

 

First of all, Happy New Year, 

 

Today the VD66GY and VD55G1 are released regarding STM32N6 We work to add ASAP the other sensor and provide code example. It is one of the priority.

 

We work also to provide libcamera + ST driver on STlinux it will be in a second time after STM32N6 

 

Regards 

Cyril Liotard 

 

 

Will_Robertson
Associate III
June 1, 2025

Hi Cyril,

I was wondering if there were any updates on development of the Linux drivers for the ST image sensors?

We'd like to look at using ST RGB and RGB-IR image sensors with libcamera and embedded Linux in the new open source wildlife camera system WildCamera - the exceptionally good RGB and IR performance of ST image sensors will deliver significantly better performance than existing proprietary wildlife cameras systems.

There's more about our work here

https://new-homes-for-old-friends.cairnwater.com/

and more detailed analysis of how user requirements translate to decisions on implementation here:

https://github.com/William-Robert-Robertson/WildCamera

Thank you very much,

Will

MeganeG
ST Technical Moderator
July 10, 2025

Hi @Will_Robertson,

We have Linux drivers available for the VD66GY RGB camera and the VD16GZ RGB-IR camera.

Here are the links to the drivers for both sensors: VD66GY , VD16GZ.

I hope this is what you were looking for!

Regards, Megane

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
asdfasdf
Associate III
February 17, 2025

Hi @CyrilTechPro ! May I ask where the drivers for VD55G1 for the STM32N6 have been released? I could not find them anywhere.

Thanks a lot,

Michael

MeganeG
ST Technical Moderator
February 27, 2025

Hi @asdfasdf,

You can find all the drivers for the STM32N6 on this page: link.

Please note that not all of our cameras are supported yet, but they will be in the coming months. However, the VD55G1 is currently supported.

Thanks, Megane.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
asdfasdf
Associate III
June 24, 2025

Hey @MeganeG !

May I kindly ask whether there is any news regarding the VD55G0 driver for the STM32N6? This has now been a few month ago, so given that this is a priority for ST maybe there already is some progress? So far I still could only find drivers for the VD55G1 (for the N6).

Thanks a lot,

Michael

asdfasdf
Associate III
February 28, 2025

Hi @MeganeG ! Is the driver also available somewhere else in stand-alone form, like the Linux drivers?

Sadly all downloads on the site you linked to do not work, the "Request download" form cannot be submitted, the "Confirm Request" button is dead - see attached screenshot.

Best, Michael

Bildschirmfoto 2025-02-28 um 07.53.31.png

MeganeG
ST Technical Moderator
March 1, 2025

Hi @asdfasdf,

No, we do not have it available in stand-alone form. All the drivers can be found at this link.

It should work normally; we have not encountered any issues on our side. Could you try accessing it on a different machine, disable all adblockers, or try using a different browser?

Let me know if it still doesn't work. If needed, I can share the drivers directly here.

Thanks, Megane.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
asdfasdf
Associate III
March 1, 2025

Dear @MeganeG ! Today, the stars aligned and I was able to download the software packages you mentioned - thank you very much! Looking forward to drivers for the VD55G0 being released, as that's the sensor I'm mostly interested in.

Best regards, Michael

MeganeG
ST Technical Moderator
July 8, 2025

Hi @asdfasdf,

Unfortunately, it seems the VD55G0 driver for the STM32N6 will not be available before 2026. Sorry for the inconvenience.

But yes, indeed, we do have drivers available for the VD55G1, VD56G3 and VD66GY in the meantime, if you are interested. 

Regards, Megane

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.