2024-11-26 09:13 AM
Hi,
I'm facing a weird problem: I correctly deployed a network using x-cube-ai but now I have to add a new one.
The configuration option does not open, when I click on x-cube-ai (see screenshot attacched) it stucks on waiting puntator...
How can I fix it ? I tried restarting STM32CUBE IDE and also restarting PC, problem persists...
IDE version 6.12.1
Regards
2024-11-27 12:27 AM
Hello @Marco27293,
First, the strange thing in your screenshot is that you are not in the "Pinout & Configuration" panel, but in the "Clock Configuration"... Is it possible to try opening your project on another pc?
It may be an issue with the window, did you try to resize the window in the middle (the one bugged). Maybe increasing its size can help...
You can try to open the .ioc file in your project directly with STM32CubeMX
Are you using the last version of cubeAI?
Have a good day,
Julian