Skip to main content
GanesanGuru
Associate II
September 1, 2022
Solved

STM32CubeAI-Keras Sequential model with multiple inputs gives INTERNAL ERROR: unpack_from requires a buffer of at least 4 bytes

  • September 1, 2022
  • 1 reply
  • 1353 views

I've followed this tinyML for stm32 from Digikey "TinyML: Getting Started with STM32 X-CUBE-AI | Digi-Key Electronics" reference,and got no Errors in STM32CubeMX when I clicked "Analyze" button after I've uploaded the tfLitemodel.

Later I've tried this

import tensorflow as tf

from tensorflow.keras.layers import *

from tensorflow.keras.models import Sequential, Model

from tensorflow.keras.optimizers import Adam, RMSprop

import numpy as np

input1 = Input(shape=(1,))

input2 = Input(shape=(1,))

input = Concatenate()([input1, input2])

x = Dense(2)(input)

x = Dense(1)(x)

model = Model(inputs=[input1, input2], outputs=x)

model.summary()

model.compile(

    optimizer = RMSprop(lr=0.02,rho=0.9,epsilon=None,decay=0),

    loss = 'mean_squared_error'

)

x1=np.array([2600, 3000, 3200, 3600, 4000 ,4100])

x2=np.array([3.0 ,4.0,4.0,3.0, 5.0,6.0])

y=np.array([550000,565000,610000, 595000,760000,810000])

history = model.fit([x1, x2], y,epochs=500)

model.predict([np.array([3000]),np.array([4])])

The python code executes without error and even prediction is working fine. Yet when I've uploaded this tfLite model in stm32cubeMX and went for "Analyze" button , I get "INTERNAL ERROR: unpack_from requires a buffer of at least 4 bytes"

PS : I'm using stm32 x-cube-ai : 5.1.2 version

Also, the reference code uses Sequential Model, while my code doesn't

This topic has been closed for replies.
Best answer by GanesanGuru

It got resolved, when using latest version of stm32 x-cube-ai (i.e.) 7.2.version

1 reply

GanesanGuru
GanesanGuruAuthorBest answer
Associate II
September 1, 2022

It got resolved, when using latest version of stm32 x-cube-ai (i.e.) 7.2.version