Skip to main content
TSchi.2269
Associate III
December 24, 2019
Solved

Interrupt behavior of LSM6DSOX?

  • December 24, 2019
  • 1 reply
  • 719 views

I am looking to create a project where I can set/latch the interrupt pin INT1 on high when the LSM6DSOX is detecting state X (where X is state 1/2/3 etc.) and goes down (low) when in a generic/static state (state 0). How is this possible? I found in one of the application notes that the PAGE_RW flag (17h) has something to do with the flag. However, I am not able to find how I can customize the output signal like described above.

Has anyone experience with interrupts and how should one do this?

This topic has been closed for replies.
Best answer by Eleon BORLINI

Hi @TSchi.2269​ , is this topic related to this thread? Regards

1 reply

Eleon BORLINI
Eleon BORLINIBest answer
ST Employee
April 3, 2020

Hi @TSchi.2269​ , is this topic related to this thread? Regards