Skip to main content
Maxime MARCHETTO
ST Community Manager
March 16, 2026

STM32CubeIDE for Visual Studio Code

Related products:STM32 software tools
  • March 16, 2026
  • 2 replies
  • 3562 views

The March 2026 release of STM32CubeIDE for Visual Studio Code is a key part of the STM32C5 series launch and the wider evolution of the STM32Cube ecosystem. Together with the new STM32CubeMX2 configuration tool and the updated STM32CubeIDE and STM32CubeIDE for VS Code integrations, this release is designed to provide seamless development experience for the next generation of STM32 MCUs.

ST thanks the developer community for their feedback and patience as the team continues to build tools for VS Code.
 

Highlights of the March 2026 update

STM32 View update: faster access to tools and resources in VS Code

The latest STM32 View update introduces new shortcuts that help developers launch tools and find documentation more efficiently.

 New shortcuts allow you to:

  • Import STM32Cube examples
    Bring STM32Cube example projects into VS Code in just a few clicks.
    Limitation: only single-core‑ STM32CubeIDE/Eclipse projects are supported.
  • Convert STM32CubeIDE/Eclipse projects
    Convert native STM32CubeIDE/Eclipse projects to CMake and import them into VS Code.
  • Explore the STM32 MCU portfolio
    Quickly browse the STM32 MCU portfolio from within your development environment.
  • Access the online example library
    Open the new STM32 example library portal to discover and reuse ready-to‑-run‑ code.

 

Maxime_MARCHETTO1_0-1773647374999.png


VS Code documentation now available online

The STM32 VS Code User Guide is now accessible online at STM32CubeIDE for Visual Studio Code.

This update means developers can:

  • Access the documentation without installing the tool
  • Deep-link directly to specific chapters from other pages, emails, or support content

Please note: the online documentation is still under development and will continue to be updated and expanded.


Native macOS AArch64 support

STM32 VS Code integration now offers native AArch64 support on macOS.
The dependency on x86_64 binaries has been removed, so:

  • Apple silicon users no longer need the Rosetta emulation layer
  • Performance and responsiveness are improved when developing on M1/M2/M3‑based Macs


Updated Bundle Manager GUI

The Bundle Manager interface has been redesigned to provide a more intuitive, developer friendly experience.

With the new GUI, developers can:

  • Install and manage multiple tool versions
    Easily add different versions of tools such as CMake, GCC, and SEGGER J‑LINK.
  • Lock tool versions per project
    Each project can pin the exact tool versions it requires, ensuring a reproducible and shareable tool environment across teams and machines.

Maxime_MARCHETTO1_1-1773647375005.png


Toolchain updates

The latest release brings significant improvements to both GCCbased and ‑Clangbased‑ toolchains for STM32 developers.


GNU Tools for STM32 (GCC 14.3.1)

  • Native AArch64 package for macOS
    Faster builds on Apple silicon thanks to native support (no Rosetta required).
  • Newlib rebuilt with -O2
    Improved runtime performance from optimized C library builds.
  • More details online
    Full release notes are available in the online documentation.


ST Arm Clang (Clang 21.1.1)

  • Better standards conformance and optimization
    Enhanced code generation quality and language compliance.
  • Improved modern C/C++ support
    Better support for C++20/23 and C23, along with upgraded diagnostics and static analysis.
  • Updated C libraries
    Includes Picolibc 1.8.10 and Newlib 4.5.0 for more robust embedded C support.


Project conversion and import

New tools make it easier to bring existing STM32 projects into VS Code by converting native STM32CubeIDE/Eclipse projects to CMake.

These features enable developers to:

  • Migrate projects from STM32CubeIDE/Eclipse to STM32CubeIDE for VS Code
  • Import ST example projects delivered in STM32CubeIDE/Eclipse format directly into VS Code

Picture2.png

 Picture3.png

 

Limitation:  multi-context projects (dual‑-core‑, TrustZone, etc.) and pre/post-build‑ steps are not currently supported.


Debug enhancements

RTOS debug views now display information in horizontal tables instead of vertical tree views, making task and resource data easier to scan and compare.

This is the first major enhancement since the initial launch in May 2025. Developers who prefer the RTOS views from the open‑source mcu-debug extensions can continue to use them, as ST upstreams debug support for ST‑LINK and SEGGER DAPs into those projects.

Maxime_MARCHETTO1_4-1773647375046.png


The Registers view now provides visualization of Cortex core registers, SysTick, NVIC, and more.

Developers can also export register contents to XML for offline analysis, debugging, or documentation.

Maxime_MARCHETTO1_5-1773647375052.png

 

Your feedback is essential in shaping the future of STM32Cube for Visual Studio Code and helping us tailor it precisely to your requirements. We look forward to reading your ideas and questions on our community forum!


Additional resources

First published on Mar 16, 2026

2 replies

Ahmet Yasin CİVAN
Associate III
April 17, 2026

Great news, thank you so much to the entire ST team involved!

After the classic Eclipse-based IDE, officially stepping into a modern, fast environment with a massive extension ecosystem like Visual Studio Code is incredibly valuable for us embedded system developers. This was one of the most highly anticipated developments in the community for a long time.

I cannot wait to migrate my projects to VS Code and try out this new extension. Thanks again for aligning the ecosystem with modern development trends. Keep up the great work and I look forward to future updates!

Associate
May 5, 2026

In the new vscode update on:

Version: 1.118.1 (Universal)
Commit: 034f571df509819cc10b0c8129f66ef77a542f0e
Date: 2026-04-29T17:36:44+03:00
Electron: 39.8.8
ElectronBuildId: 13870025
Chromium: 142.0.7444.265
Node.js: 22.22.1
V8: 14.2.231.22-electron.0
OS: Darwin arm64 25.4.0

STM32cudeide can not work!

[proc] 正在执行命令: cube-cmake --version
[proc] 命令: cube-cmake --version 失败,出现错误: Error: spawn cube-cmake ENOENT
截屏2026-05-05 上午9.50.55.png