Skip to main content
RSeba.2
Associate III
July 25, 2023
Question

SPI Communication SPC58EC MCU

  • July 25, 2023
  • 6 replies
  • 3584 views

Hello,

Currently I am working with SPI communication in SPC58EC DISP Discovery board. I wanted to evaluate communication between  MS-SL and SL-MS. I have configured SPID1 as master and SPID2 as slave. I was able to send data from master to slave using  below functions. 
spi_lld_receive(&SPID2, TRANSFER_BUFFER_SIZE, &spihandler_rx_fifo);
spi_lld_send(&SPID1, TRANSFER_BUFFER_SIZE, transmitBuff);
But how can I transmit data from slave to master ? Can I use the same functions for it or should I use spi_lld_exchange?

Thanks and regards.

This topic has been closed for replies.

6 replies

TDK
July 25, 2023

spi_lld_exchange is a two-way SPI transfer which can work. Note that the master has to initiate all transfers. That is to say, spi_lld_exchange/spi_lld_send on the slave must be called before spi_lld_exchange/spi_lld_receive is called on the master.

"If you feel a post has answered your question, please click ""Accept as Solution""."
RSeba.2
RSeba.2Author
Associate III
July 26, 2023

Thanks for this information. But I couldn't receive all the data that I sent out from slave in master. 
I have used the following configuration.

const SPIConfig spi_config_master = {
SPI_MASTER,
0,
PORT_E,
8,
0UL | SPC5_CTAR_FMSZ(8) |
SPC5_CTAR_PCSSCK_PRE1 | SPC5_CTAR_PASC_PRE1 |
SPC5_CTAR_PDT_PRE1 | SPC5_CTAR_PBR_PRE2 |
SPC5_CTAR_CSSCK_DIV4 | SPC5_CTAR_ASC_DIV4 |
SPC5_CTAR_DT_DIV2 | SPC5_CTAR_BR_DIV2,
0UL | SPC5_PUSHR_CONT | SPC5_PUSHR_CTAS(0) | SPC5_PUSHR_PCS(1)
};

/**
* @brief Structure defining the SPI configuration "slave".
*/
const SPIConfig spi_config_slave = {
SPI_SLAVE,
0,
PORT_A,
4,
0UL | SPC5_CTAR_FMSZ(8) ,
0
//0UL | SPC5_PUSHR_CONT | SPC5_PUSHR_CTAS(0) | SPC5_PUSHR_PCS(0)
};
 I have used the following functions.

spi_lld_send(&SPID2, TRANSFER_BUFFER_SIZE, transmitBuff); //slave transmit
spi_lld_receive(&SPID1, TRANSFER_BUFFER_SIZE, &spihandler_mrx_fifo);

Do you know what might be the problems?

RSeba.2
RSeba.2Author
Associate III
July 26, 2023
TDK
July 26, 2023

How are you ensuring the slave calls its SPI transfer function before the master calls its SPI transfer function?

"If you feel a post has answered your question, please click ""Accept as Solution""."
RSeba.2
RSeba.2Author
Associate III
July 27, 2023

case 'a':

debug_print_string("Starting SPI frame transmission from master:");
debug_print_crlf();
debug_print_string("Test case for command: FRCMD_GET_STATUS ");
debug_print_crlf();

tfsend_prepare(&tfc_spihandler, TF_ID_COMMAND, FRCMD_GET_STATUS);
tfsend_flush(&tfc_spihandler);
spi_lld_send(&SPID1, TRANSFER_BUFFER_SIZE, transmitBuff);

/* Slave transmit */
for (int i = 0; i < TRANSFER_BUFFER_SIZE; i++) {
transmitBuff_test[i] = 0x11;
}
spi_lld_send(&SPID2, TRANSFER_BUFFER_SIZE, transmitBuff_test);  //slave

spi_lld_receive(&SPID1, TRANSFER_BUFFER_SIZE, &spihandler_mrx_fifo); //master

break;


Case 'a' is input from the keyboard. When I press 'a', above code is executed.
Here, spi_lld_send(&SPID2, TRANSFER_BUFFER_SIZE, transmitBuff_test) of slave is called                                     before master receive function spi_lld_receive(&SPID1, TRANSFER_BUFFER_SIZE, &spihandler_mrx_fifo);