Skip to main content
JWeij.1
Visitor II
March 10, 2020
Question

Best Low Power buffer op amp

  • March 10, 2020
  • 1 reply
  • 1022 views

I need to measure a signal with very low power, the signal can range anywhere between -1 and +10 Volts but i only need the 0 to 3volts for my ADC input(my battery is also 3V). is there an opamp that fits my requirements that is less than 50uA?

This topic has been closed for replies.

1 reply

MikeDB
Senior II
March 17, 2020