Skip to main content
Nicholas Parker
Associate III
April 16, 2018
Question

ADC -> digital filter -> I2S Audio

  • April 16, 2018
  • 4 replies
  • 2146 views
Posted on April 17, 2018 at 00:49

I'm using the STM32F407 Discovery Board to implement a digital band pass filter, this board has a CS43L22 Audio DAC which I want to use for output, (not in analog pass through mode).

However, this seems to create a challenge as the data flow to the DAC must have a continuous clock signal from the STM32F407, so this means the DAC update  rate sets the rate at which I'd need to sample using the STM32F4's on-board ADC.

Is there a clean mechanism / way to use an ADC on the STM, at an arbirtary rate (set by a timer used as a trigger source) and then do some filtering, then pass the data to the I2S DAC?

The only way I can think, is to have the CL43L22 clocked continuously at 'some' rate with data being sent over I2S being supplied from a couple of data (L and R channel) ram variables, which I update from my filter asynchronously (when its ready).

Is there a better way?

    This topic has been closed for replies.

    4 replies

    MDoro
    Associate
    November 11, 2018

    Hi could you solve that? I have same problem.  In my project Im reading samples with the adc at 48Khz using timer interrupts and adcConvCallbacks, load them in a buffer of 256 samples and when the buffer is full I send it via i2s to the DAC . Im using two buffers, when the bufferA is full i send it and start saving samples in the bufferB, when its full I swap again so I have 256 samples available at any time. 

    My problem is that en every swap of buffers I heard a "plop" noise from the dac. Do you know how can I avoid that? It seems to sound at every time that a new buffer is sended via HAL_I2S_Transmit() . Im not using interrupts in the I2s, just call it at every time I have a full buffer. 

    SUl H
    Associate
    November 15, 2018

    kindly share the adc audio input code with me i am doing same type of work but dnt know how to get audio input to do further processing on it like band pass filtering.

    thankyou

    MDoro
    Associate
    November 15, 2018

    Yes of course, this is the code. I have another version using interrupts in the i2s transmition but i havent uploaded it to my github yet. Please let me know if you figure out how to eliminate the "plop". I think its becouse there is a sort of de-sinchronization in the buffers swap.

    https://github.com/maximdorogov/Digital-Audio/blob/master/Src/main.c

    SUl H
    Associate
    November 16, 2018
    • would it work in Keil??? i want to use keil mdk using cube mx ???
    • Like
    • Reply
    •  

    SUl H
    Associate
    November 16, 2018

    would it work in Keil??? i want to use keil mdk using cube mx ???

    mccartneydamon
    Associate
    May 10, 2020

    Did you ever solve this issue?

    D