Skip to main content
Associate
Mar 8, 2024 1:18 AM UTC
Solved

X-NUCLEO-LPM01A board not found on Windows 10 or MAC

i've installed versions of STM32CubeProgrammer on my windows 10 PC as well as my MAC....

i'm following the instructions in um2269 (section 8) on updating firmware, but see a message saying "No DFU detected" under the USB configuration panel....  selecting Connect fails at that point....

on windows, the device manager seems to identify a 'Power Shield (Virtual ComPort in FS Mode)' as well as a new 'USB Serial Device' when i plug in my board....  but there is a warning sign that ultmately tells me that windows can't find a driver....  drivers were definitely installed along with CubeProgrammer; and i've run some .bat file under the Drivers folder....

do i need to do anything with my (brand new) board???  if i move the sliding jumper to the 'Syst' position *BEFORE* plugging in the board, it doesn't even power up....

 

This topic has been closed for replies.
biosbobBest answer
Associate
Mar 8, 2024 9:57 PM UTC

you really *DO* need to slide that jumper in the 'Syst' position before plugging in the board -- even if the board appears dead....

all's well after updating the firmware to the latest version....

1 reply

biosbobAuthorBest answer
Associate
Mar 8, 2024 9:57 PM UTC

you really *DO* need to slide that jumper in the 'Syst' position before plugging in the board -- even if the board appears dead....

all's well after updating the firmware to the latest version....