Skip to main content
YLU.2
Associate
Apr 25, 2023 5:44 AM UTC
Question

write flash fail via i2c bootloader

Recently I'm using STM32G051 and try to write flash via i2c bootloader.

Below are my steps:

  1. Use STM32CubeProgrammer to set nBOOT0_SEL = 1 / nBoot0 = 0 /nBoot1 = 1 to enter BL mode
  2. Disconnect ST link, and use i2c host tool (Aardvark) to send i2c write (no-stretch) command 0x32, 0xcd
  3. Read 1 byte, get ACK (0x79) frame successfully.
  4. Send 5 bytes start address(0x08000000) with XOR checksum (0x08)
  5. Read 1 byte, get ACK (0x79) frame successfully.
  6. send 10 bytes writeLength(0x08), data(0x11,0x22,0x33,0x44,0x55,0x66,0x77,0x88), checksum (0x80)
  7. Problem here!! read 1 byte and expect to get ACK(0x79) or BUSY(0x76), but I saw CLK is stretched at 9th bit of address phase:
    _legacyfs_online_stmicro_images_0693W00000bikrMQAQ.png

I've checked all read/write protection are disabled via STM32Programmer, and I can access read flash and erase flash successfully, only write process fail. Is any one have encounter similar issue and tell me if my procedure is not correct?

Many thanks.

This topic has been closed for replies.

6 replies

Senior III
Apr 25, 2023 8:07 AM UTC

Hi,

flash memory start form address 0x0800 0000 not 0x0008 0000. You passed addres that is marked as reserved.


_legacyfs_online_stmicro_images_0693W00000bilVgQAI.png

Dudo
YLU.2
YLU.2Author
Associate
Apr 25, 2023 8:20 AM UTC

Hi Kamil,

Sorry for my typo, I've written the start address with 0x08000000 and the XOR checksum (0x08)

And still have the issue.

Thanks.

YenLu

Senior III
Apr 25, 2023 9:24 AM UTC

Ok :) Next question, were you send bootloader address ? in application note i see other adressess than yours. What is this sequention 0x32 0xcd?


_legacyfs_online_stmicro_images_0693W00000bilulQAA.png

Dudo
YLU.2
YLU.2Author
Associate
Apr 25, 2023 12:51 PM UTC

Hi Kamil,

I omitted the i2c address byte when I described the step above. I've read/write the address 0x62 and everything is fine until waiting the ack response for data written. The sequence (0x32, 0xcd) is No-Stretch Write Memory command which is described in AN4221:


_legacyfs_online_stmicro_images_0693W00000bimpwQAA.png 

Senior III
Apr 27, 2023 8:45 AM UTC

@YLU.2​ did you resolve problem?

Dudo
YLU.2
YLU.2Author
Associate
Apr 28, 2023 3:25 AM UTC

Yes,

for 8 byte write, I should send 0x07, 0x11,0x22,0x33,0x44,0x55,0x66,0x77,0x88, 0x8f

after correct the format, I get ack and write the memory successfully.