Skip to main content
Senior
Jul 7, 2026 2:44 PM UTC
Question

Where Did nSWBOOT0 Go?

Previously I used Programmer v2.15 on H5 MCUs to zero (uncheck) nSWBOOT0. Probably due to Windows drivers updates, I could no longer connect.

I updated to Programmer v2.23 and I can now connect, but I no longer see nSWBOOT0 anywhere. Where did it go?

2 replies

KDJEM.1
ST Technical Moderator
Jul 8, 2026 12:29 PM UTC

Hello ​@mccabehm ;

 

Which STM32 are you using STM32G0 or STM32H5?

Could you please share the device number? 

According references manuals, the nSWBOOT0 bit isn’t supported in STM32G0 and STM32H5 devices.

I recommend you to look at Introduction to system memory boot mode on STM32 MCUs - Application note application note to boot from system memory.

 

Thank you. 

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
mccabehmAuthor
Senior
Jul 8, 2026 1:24 PM UTC

STM32H563. Yes, I see that the reference manual has no mention of nSWBOOT0.

Apparently Programmer v2.15 displayed nSWBOOT0 (I know I saw it); and v2.23 doesn’t display it.

Then any change in behavior I thought I saw after unchecking nSWBOOT0 was imaginary 🙂