Skip to main content
Entony
Associate II
Dec 16, 2021 9:57 AM UTC
Solved

We have a problem downloading to the STM32L100 processor. It was programmed using STLink. Now we want to use STM32CubeProgrammer. Writing is not possible! It is not possible to change the RDP value either. If we use STLink, all is OK.

 10:55:25 : ST-LINK SN : 0034003E3137510339383538

 10:55:25 : ST-LINK FW : V3J8M3B5S1

 10:55:25 : Board    : STLINK-V3MODS

 10:55:25 : Voltage   : 3.29V

 10:55:25 : SWD freq  : 8000 KHz

 10:55:25 : Connect mode: Under Reset

 10:55:25 : Reset mode : Software reset

 10:55:25 : Device ID  : 0x429

 10:55:25 : Revision ID : Rev Y

 10:55:25 : UPLOADING OPTION BYTES DATA ...

 10:55:25 :  Bank     : 0x00

 10:55:25 :  Address    : 0x40023c1c

 10:55:25 :  Size     : 136 Bytes

 10:55:25 :  Bank     : 0x01

 10:55:25 :  Address    : 0x1ff80000

 10:55:25 :  Size     : 136 Bytes

 10:55:25 : UPLOADING ...

 10:55:25 :  Size     : 1024 Bytes

 10:55:25 :  Address    : 0x8000000

 10:55:25 : Read progress:

 10:55:25 : Data read successfully

 10:55:25 : Time elapsed during the read operation is: 00:00:00.003

 10:55:51 : Option byte command : -ob RDP=187 

 10:55:51 : PROGRAMMING OPTION BYTES AREA ...

 10:55:51 :  Bank     : 0x01

 10:55:51 :  Address    : 0x1ff80000

 10:55:51 :  Size     : 136 Bytes

 10:55:51 : Reconnecting...

 10:55:52 : Reconnected !

 10:55:52 : UPLOADING OPTION BYTES DATA ...

 10:55:52 :  Bank     : 0x00

 10:55:52 :  Address    : 0x40023c1c

 10:55:52 :  Size     : 136 Bytes

 10:55:52 :  Bank     : 0x01

 10:55:52 :  Address    : 0x1ff80000

 10:55:52 :  Size     : 136 Bytes

 10:55:52 : OPTION BYTE PROGRAMMING VERIFICATION:

 10:55:52 : Error: Expected value for Option Byte "RDP": 0xBB, found: 0xAA

 10:55:52 : Error: Option Byte Programming failed

This topic has been closed for replies.
Imen.DBest answer
ST Technical Moderator
Dec 16, 2021 11:05 AM UTC

Hello @Entony​ and welcome to the Community :)

What Cubeprogrammer version are you used ? Please make sure to use the latest release.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

2 replies

Imen.DBest answer
ST Technical Moderator
Dec 16, 2021 11:05 AM UTC

Hello @Entony​ and welcome to the Community :)

What Cubeprogrammer version are you used ? Please make sure to use the latest release.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Entony
EntonyAuthor
Associate II
Dec 17, 2021 6:39 AM UTC

We had an old version, v2.8.0. Now we have a new version v2.9.0 and it works fine!

Thanks for the warning and I'm sorry, that should have occurred to me.;)