Skip to main content
TCash.1
Associate III
Oct 26, 2020 10:37 PM UTC
Question

Verification Failed On UART Programming STM32CubeProgrammer

Hello,

I am trying to program the STM32H743ZI using the STM32CubeProgrammer tool in uart mode.

First in order to get the board into the boot loader I use the following runtime code to get into bootloader mode:

/**
 * Function to perform jump to system memory boot from user application
 *
 * Call function when you want to jump to system memory
 */
void JumpToBootloader(void) {
 
 
	 uint32_t i=0;
	 void (*SysMemBootJump)(void);
 
	 /* Set the address of the entry point to bootloader */
	 volatile uint32_t BootAddr = 0x1FF09800;
 
	 /* Disable all interrupts */
	 __disable_irq();
 
	 /* Disable Systick timer */
	 SysTick->CTRL = 0;
 
	 /* Set the clock to the default state */
	 HAL_RCC_DeInit();
 
	 /* Clear Interrupt Enable Register & Interrupt Pending Register */
	 for (i=0;i<5;i++)
	 {
		 NVIC->ICER[i]=0xFFFFFFFF;
		 NVIC->ICPR[i]=0xFFFFFFFF;
	 }
 
	 /* Re-enable all interrupts */
	 __enable_irq();
 
	 /* Set up the jump to booloader address + 4 */
	 SysMemBootJump = (void (*)(void)) (*((uint32_t *) ((BootAddr + 4))));
 
	 /* Set the main stack pointer to the bootloader stack */
	 __set_MSP(*(uint32_t *)BootAddr);
 
	 /* Call the function to jump to bootloader location */
	 SysMemBootJump();
 
	 /* Jump is done successfully */
	 while (1)
	 {
	 /* Code should never reach this loop */
	 }
}

Then I connect via UART3 to the chip and try to program it. It seems to transfer the program ok - but fails on verifying. The same result happens at different lower baudrates as well. Below is the output of STM32_Programmer_CLI.exe:

" -------------------------------------------------------------------\r\n STM32CubeProgrammer v2.4.0 \r\n -------------------------------------------------------------------\r\n\r\nSerial Port COM20 is successfully opened.\r\nPort configuration: parity = even, baudrate = 115200, data-bit = 8,\r\n stop-bit = 1.0, flow-control = off\r\nActivating device: OK\r\nChip ID: 0x450 \r\nBootLoader protocol version: 3.1\r\n\r\n\r\nMemory Programming ...\r\nOpening and parsing file: DSPBoardH7.elf\r\n File : DSPBoardH7.elf\r\n Size : 92232 Bytes\r\n Address : 0x08000000 \r\n\r\n\r\nErasing memory corresponding to segment 0:\r\nDownload in Progress:\r\n\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1 0%\r\xDB 2%\xDB 4%\xDB 6%\xDB 8%\xDB 10%\xDB 12%\xDB 14%\xDB 16%\xDB 18%\xDB 20%\xDB 22%\xDB 24%\xDB 26%\xDB 28%\xDB 30%\xDB 32%\xDB 34%\xDB 36%\xDB 38%\xDB 40%\xDB 42%\xDB 44%\xDB 46%\xDB 48%\xDB 50%\xDB 52%\xDB 54%\xDB 56%\xDB 58%\xDB 60%\xDB 62%\xDB 64%\xDB 66%\xDB 68%\xDB 70%\xDB 72%\xDB 74%\xDB 76%\xDB 78%\xDB 80%\xDB 82%\xDB 84%\xDB 86%\xDB 88%\xDB 90%\xDB 92%\xDB 94%\xDB 96%\xDB 98%\xDB 100%\r\n\r\nFile download complete\r\nTime elapsed during download operation: 00:00:23.082\r\n\r\n\r\n\r\nVerifying ...\r\n\r\n\r\nRead progress:\r\n\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1\xB1 50%\r\r\n\r\nError: Read Serial Response timed out.\r\n\r\n\r\nError: Error occured during memory read at address 0x08000200\r\n\r\n\r\nError: Failed to read memory at address 0x08000000 during verification\r\n\r\n\r\nError: Download verification failed\r\n\r\n\r\n\r\nRUNNING Program ... \r\n Address: : 0x8000000\r\n\r\nTimeout error occured while waiting for acknowledgement.\r\nError: START command not acknowledged!\r\nError: Start operation failed\r\n"

Any Ideas on how to fix this or what I'm missing would be appreciated!

This topic has been closed for replies.

3 replies

STOne-32
ST Technical Moderator
Oct 31, 2020 9:06 PM UTC

can you try to enter boortlaoder mode by hardware option instead of run-time ? and check again.

as it seems not able to read at start of the flash at address 0x0800_0000 which is the run-time bootstrap code.

TCash.1
TCash.1Author
Associate III
Nov 2, 2020 7:33 PM UTC

HI STOne-32,

I was able to enter bootloader mode by hardware (holding boot0 high and pulling down the reset pin to reset the board). And indeed I was able to program and verify with UART once in that state.

I'm guessing not, but Is there a way that the chip can be programmed in software boot mode? Basically I need a way for the H7 to get itself into boot mode. Is using the chip to drive its own boot0 via external pins a better method for this?

Thanks for your help

TCash.1
TCash.1Author
Associate III
Nov 2, 2020 8:17 PM UTC

Update: I was able to have the H7 drive its own BOOT0 pin high via another pin and a capacitor for holding it high long enough for self reset (again via an external pin). This seems to work well for me