Skip to main content
rtl
Associate II
Nov 29, 2022 10:24 AM UTC
Solved

Using the STM32CubeProgrammer API

Hello!

I am trying to use the STM32CubeProgrammer API to create my own application with a simple GUI in C++. Currently my solution is compiling the STM32CubePrgAPI as static library and then include it in a MFC project.

Basically user clicks OK from the GUI and then Example2 is executed. The getSTLinkList function executes with no issues, but connectSTLink fucktion gives me this error.

int connectStlinkFlag = connectStLink(debugParameters);
 
0xC0000005: Access violation executing location 0x0000000000000000.

If I compile STM32CubePrgAPI as .exe, it works with no problems.

What am I not understanding? Is compiling it as a static library a valid choice? What other options do I have?

I can't find any examples of applications created using this API. Has anyone done something like this?

This topic has been closed for replies.
rtl
rtlBest answer
Associate II
Nov 29, 2022 11:31 AM UTC

Initially I excluded the progress bar and message display functions callbacks, because I thought they weren't needed for my use case as I am not using the CLI. Apparently it is needed and adding it fixed my issue. Can anyone explain, why?

/**
 * \brief This routine allows to choose your custom display.
 * \param c : Fill the struct to customize the display tool.
 * \note This function must be called first of all to ensure the display management.
 */
void setDisplayCallbacks(displayCallBacks c);

 displayCallBacks vsLogMsg;
 
 /* Set the progress bar and message display functions callbacks */
 vsLogMsg.logMessage = DisplayMessage;
 vsLogMsg.initProgressBar = InitPBar;
 vsLogMsg.loadBar = lBar;
 setDisplayCallbacks(vsLogMsg);

1 reply

rtl
rtlAuthorBest answer
Associate II
Nov 29, 2022 11:31 AM UTC

Initially I excluded the progress bar and message display functions callbacks, because I thought they weren't needed for my use case as I am not using the CLI. Apparently it is needed and adding it fixed my issue. Can anyone explain, why?

/**
 * \brief This routine allows to choose your custom display.
 * \param c : Fill the struct to customize the display tool.
 * \note This function must be called first of all to ensure the display management.
 */
void setDisplayCallbacks(displayCallBacks c);

 displayCallBacks vsLogMsg;
 
 /* Set the progress bar and message display functions callbacks */
 vsLogMsg.logMessage = DisplayMessage;
 vsLogMsg.initProgressBar = InitPBar;
 vsLogMsg.loadBar = lBar;
 setDisplayCallbacks(vsLogMsg);