Skip to main content
BSchm.6
Associate II
May 25, 2023 12:14 PM UTC
Solved

Use STM CubeProgrammer with Jlink?

Hi,

during development I work with the CubeIDE and use JLink, it connects to the SWD-port of my STM-board properly and works like a charm within the IDE.

Now we're about to program loads of different boards. From my understanding this is where the CubeProgrammer shoukd be used. But when starting it, the JLink is not recognised, it only tells me about some ST-Link which could not be found (which is correct as it does not exist).

So how/where do I have to configure the CubeProgrammer to work with the JLink?

Thanks!

This topic has been closed for replies.
Pavel A.
Pavel A.Best answer
May 25, 2023 6:44 PM UTC

Unlike CubeIDE, the CubeProgrammer  does not work with J-Link. But you can use the Segger J-Flash software for the same price.

3 replies

Pavel A.
Pavel A.Best answer
May 25, 2023 6:44 PM UTC

Unlike CubeIDE, the CubeProgrammer  does not work with J-Link. But you can use the Segger J-Flash software for the same price.

Explorer
Oct 15, 2024 1:11 AM UTC

I just connected to a target using CubeMXProgrammer v2.17.0 connected via a J-Link. 

Associate III
May 23, 2024 10:18 AM UTC

Since CubeProgrammer 2.16.0 it is supported, you may update the answer.

 

See also other post .