Skip to main content
sasha
Associate III
Oct 30, 2019 5:57 AM UTC
Question

USB DFU Error Uploading Option Bytes, and incorrect serial number reported - STM32F746

We have custom hardware with STM32F746, and having issues getting factory bootloader DFU USB working. When I run STM32_Programmer_CLI -l usb command, I can see my device (although Serial Number looks wrong).

0690X00000ArQiAQAV.jpg

When I try to connect with STM32CubeBootloader (tried V2.1 and V2.2), I get the following errors:

16:19:53:063 : Error: Uploading Option Bytes bank: 0 failed

16:19:53:091 : Error: Initializing the Option Bytes failed

0690X00000ArQiUQAV.jpg

My board has a 24MHz external crystal.

Does anyone know what the issue might be?

I think the correct drivers are installed.

0690X00000ArQieQAF.jpg

This topic has been closed for replies.

5 replies

Nesrine.JLASSI
Visitor II
Nov 4, 2019 3:04 PM UTC

Hello @sasha​ 

Try to repeat the same scenario with the latest version of CubeProgrammer . I just tested it now and did not have any problems.

0690X00000Aren9QAB.png

Best regards,

Nesrine

sasha
sashaAuthor
Associate III
Jan 24, 2020 7:00 AM UTC

Hi, I am still having issues with this. I have tried with version 2.3.0 of STM32CubeProgrammer and it has the same issue - I can connect via USB, it reports the correct Device ID and FW version, but has an incorrect Serial Number & fails to upload option bytes.

We have two hardware configuration which both have the same issue: One is clocked with 24MHz crystal, and one with 25MHz External Oscillator.

I have also tried this on two different computers - same issue.

What could be the issue?

0690X00000BwUlbQAF.jpg

sasha
sashaAuthor
Associate III
Feb 25, 2020 10:50 AM UTC

Hi again, does anyone know what happens if the internal bootloader mis-calculates the HSE frequency? I'm wondering if this could cause the issue I'm seeing.

​

Sometimes my custom PCB will work with Dfu, and sometimes it will not - it does connect, but then fails when reading the option bytes as described above. I have tested 10 different pieces if PCB - one day all of them worked with DFU, another day only 1 of them worked.

​

I see in the App Note it mentions that if the HSI calibration is out by 1% it can miscalculate and HSE value and that DFU might "dysfunction or not work at all". We are testing at 25degC.

​

Is DFU stable with 25MHz HSE clock (oscillator)? Has anyone had experience with this?

SJULI.1
Associate II
Dec 11, 2020 3:31 PM UTC

Hi Sasha, Did you find a solution? I have the problem...

HTitalia
Associate II
Mar 11, 2021 1:36 PM UTC

Hi Sasha and SJuli

did you solved your problem? I just got the error and don't know how to solve it..

Thanks.