Skip to main content
Associate III
May 6, 2024 5:13 PM UTC
Question

Unable to uninstall STM32CubeProgrammer v2.16 (Windows 11, 64-bit)

I cannot uninstall STM32CubeProgrammer v2.16 (64-bit) from my Windows 11 64-bit system.

  • If I try to uninstall it from the Windows Apps->Installed Apps list, a terminal window briefly flashes on the screen and then nothing else happens.

 

  • If I go to C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\Uninstaller and run "unscript.bat" as Administrator, I get this window:

Dazai_0-1715014870334.png

Whether or not I select "Force the deletion of ...", when I click "Uninstall," I get an unhandled exception pop-up (I can't find a way to copy the text out of it, sorry), which appears to indicate Access Denied when trying to modify registry keys:

Dazai_1-1715014974110.png

My company uses a credentials manager to provide admin privileges as needed when installing and uninstalling apps, and it asked if I wanted to escalate my privileges in both cases (running the uninstaller and running the script directly), but it said the software publisher was "Unknown" as if it didn't install correctly or wasn't signed.

I'm at a loss on what to do here; I want to try a previous version as my USB DFU device isn't identifying properly on USB when plugged in (which I see may be a common issue with 2.16), but I'm concerned about having multiple versions and drivers making this problem worse.  Any suggestions to remove Programmer 2.16?

This topic has been closed for replies.

1 reply

Aziz BRIGUI
ST Technical Moderator
May 20, 2024 10:31 AM UTC

Hello @Dazai,

Sorry for the late reply,

I could only reproduce the issue you're seeing if I was running the uninstaller with insufficient privileges. With admin rights, everything worked as expected. So could you please check with your company IT team to make sure you have sufficient privileges ? STM32CubeProgrammer is properly signed.

For having multiple versions, there should be no conflict issues, just change the installation path to something like "STMicroelectronics\STM32Cube\STM32CubeProgrammer v2.16".

Aziz

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.