Skip to main content
chrisPyres66
Associate III
Sep 5, 2019 1:05 PM UTC
Solved

UART3 BOOT MODE ON STM32H743 WITH STM32CUBPROGRAMMER V2.1.0

Dear All,

I jump in boot mode with boot0 to high level, and i can test it with dfu USB connexion.

Unfortunately, it does not work with UART3.

I have the TX signal 0x3F coming from computer, but any acknowledgment. In STM32CUBPROGRAMMER, there is : "Error: Activating device: KO. Please, verify the boot mode configuration and check the serial port configuration. Reset your device then try again..."

I use an usb - ttl 3.3v cable which works, and I did not add pull up resistor because the signal is high by default.

Any help would be greatly appreciated.

Thanks,

This topic has been closed for replies.
chrisPyres66
chrisPyres66Best answer
Associate III
Oct 24, 2019 9:41 AM UTC

It works now with stm32cubeprogrammer v2.2.0

1 reply

chrisPyres66
chrisPyres66AuthorBest answer
Associate III
Oct 24, 2019 9:41 AM UTC

It works now with stm32cubeprogrammer v2.2.0