Skip to main content
TJime.1
Associate
Nov 30, 2022 1:38 AM UTC
Solved

UART DFU on stm32l475

Hi,

I am attempting to jump to system memory to be able to update the firmware via UART. Due to design constraints, BOOT0 pin will not an option for accessing the bootloader thus jumping to system memory within the application is needed.

I'm using the following code to jump to system memory:

__enable_irq();
HAL_RCC_DeInit();
HAL_DeInit();
SysTick->CTRL = 0;
SysTick->LOAD = 0;
SysTick->VAL = 0;
 
__HAL_SYSCFG_REMAPMEMORY_SYSTEMFLASH();
 
const uint32_t p = (*((uint32_t*) 0x1FFF0000));
__set_MSP( p );
 
void (*SysMemBootJump)(void);
SysMemBootJump = (void (*)(void)) (*((uint32_t *) 0x1FFF0004));
SysMemBootJump();

In AN2606 there is a note for MCUs that use the dual bank feature, I believe this is the part that is preventing the system from bootloading correctly. I jump to system memory in main() and using STM32CubeProgrammer attempt to connect via UART. However, it timeouts since there is no response from the ST chip.

I've tried this code both on my dev kit and custom hardware with the same result.

Is there a step that I am missing in order to correctly perform a UART DFU?

Thanks,

Tom

This topic has been closed for replies.
Sara BEN HADJ YAHYA
ST Technical Moderator
Dec 8, 2022 8:30 AM UTC

Hello @TJime.1​ ,

Thanks for your feedback and welcome to STCommunity,

You can activate the bootloader by applying one of the patterns described in Table 2 in AN2606. In the case of STM32L475, check pattern 7.

Since BOOT0 is not an option for you, you can activate BFB2 Option byte and delete the flash memory (second option in pattern 7). No code is needed to jump to system memory if you decide to work with this.

I hope this helps !

If you need any further details, don't hesitate to ask me :smiling_face_with_smiling_eyes:

Sara.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

1 reply

Sara BEN HADJ YAHYA
ST Technical Moderator
Dec 8, 2022 8:30 AM UTC

Hello @TJime.1​ ,

Thanks for your feedback and welcome to STCommunity,

You can activate the bootloader by applying one of the patterns described in Table 2 in AN2606. In the case of STM32L475, check pattern 7.

Since BOOT0 is not an option for you, you can activate BFB2 Option byte and delete the flash memory (second option in pattern 7). No code is needed to jump to system memory if you decide to work with this.

I hope this helps !

If you need any further details, don't hesitate to ask me :smiling_face_with_smiling_eyes:

Sara.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.