Skip to main content
Visitor II
Jan 12, 2026 12:39 PM UTC
Question

UART Bootloader for STM32F412VGTx

As mentioned in the AN2606 document for STM32F412VGTx MCU(Custom chip), I am using USART2 (PD6/PD5) for UART bootloader using STM32CubeProgrammer. But I am getting an error message as attached. Help me to resolve this issue.

Screenshot 2026-01-09 124126.png

4 replies

Andrew Neil
Super User
Jan 12, 2026 12:43 PM UTC

Welcome to the forum.

 


@shanmukhi wrote:

STM32F412VGTx MCU (Custom chip)


STM32F412VGTx is not a custom chip.

Did you mean STM32F412VGTx on a custom board ?

If so, you need to give details of that board:

How to write your question to maximize your chances to find a solution

 


@shanmukhi wrote:

Screenshot 2026-01-09 124126.png


So have you checked those things?

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User
Jan 12, 2026 2:17 PM UTC

@Andrew Neil wrote:

Did you mean STM32F412VGTx on a custom board ?


If so, is it a known-good commercial product, or your own design?

Have you checked the design against Application note AN4488, "Getting started with STM32F4xxxx MCU hardware development" ?

Has this board ever worked ?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
TDK
Jan 12, 2026 1:54 PM UTC

One of these is likely wrong:

  • Ensure power rails are all connected correctly. All pins.
  • Ensure VCAP voltage is 1.2 V
  • Hold BOOT0 high during reset to boot into the bootloader.
  • Ensure wiring is correct.
"If you feel a post has answered your question, please click ""Accept as Solution""."
Tesla DeLorean
Guru
Jan 12, 2026 10:30 PM UTC

Any signals on PA10 or PB11 that might be recognized as initial contact?

You only get one-shot at reset to make a connection, if that fails you must with BOOT=HIGH to try again.

Present schematic for what you've implemented, saves everyone have to guess at causes..

 

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..