Skip to main content
Gneifel
Associate
Sep 16, 2020 8:04 AM UTC
Solved

"tm32cubeprog_v2-5-0": API-Error with Windows 7

Hello everybody,

I am actually a PC software developer, but would like to be able to update the firmware of the hardware we have developed with our own software.

For this purpose I have downloaded the "en.stm32cubeprog_v2-5-0.zip" and installed the Windows version on a Windows 10 (64 Bit) PC.

I tried the example "1 example with UART bootloader" from the STM-API.

This also works very well under Windows 10/64-bit.

(A Windows 10 with 32 bit is unfortunately not available to me for testing)

But when testing it with Windows 7 (32 / 64 Bit, both the same effect) I get an error when calling the API-function

"connectDfuBootloader".

Code:

   if ((usbConnectFlag = connectDfuBootloader(dfuList[0].usbIndex)) == 0)

   ...

The value in "usbConnectFlag" is then equal to "-5", which according to the API description "STM32CubeProgrammer_API.chm" means something like:

"Operation not supported or unimplemented on this interface".

When using the original GUI-programm of STM it works on Windows 7.

So the driver(s) should be OK. I hope so.

Is there any known problem/bug with Windows 7 and the API?

Or am I doing something wrong?

Please excuse me if I have not yet provided important information, but I am absolutely no expert in the embedded world ;)

Hardware:

Evaluationboard "NUCLEO F072RB"

# Update #

I have now put this question to support.

If I get a satisfactory answer there, I'll post it here.

This topic has been closed for replies.
Gneifel
GneifelBest answer
Associate
Sep 22, 2020 1:29 PM UTC

Hello again,

I found the bug and it was - how could it be otherwise? - my mistake.

The polluter:

I did not adhere to the required tree structure of the individual files completely correctly.

There must be two directories in parallel on one folder level:

The "Data_Base" directory with its xml files and a directory of any name,

in which all necessary dlls belong.

Unfortunately I had the dlls and the "Data_Base" in a common directory.

Well, ashes on my head.

But if I can help only one person who is also confused by the rigid required structure of directories,

the whole thing would ultimately have something good.

3 replies

Gneifel
GneifelAuthorBest answer
Associate
Sep 22, 2020 1:29 PM UTC

Hello again,

I found the bug and it was - how could it be otherwise? - my mistake.

The polluter:

I did not adhere to the required tree structure of the individual files completely correctly.

There must be two directories in parallel on one folder level:

The "Data_Base" directory with its xml files and a directory of any name,

in which all necessary dlls belong.

Unfortunately I had the dlls and the "Data_Base" in a common directory.

Well, ashes on my head.

But if I can help only one person who is also confused by the rigid required structure of directories,

the whole thing would ultimately have something good.

Kamil Mozdzynski
Visitor II
Nov 26, 2020 12:07 AM UTC

Hi Gneifel !

I am currently running USB_Example with the STM32Cube Programmer API and I have the exact same error. I copied the files to my own directory. I'm probably missing something. Did you mention that you need to properly configure the directory structure? What is the exact solution?

Regards,

Kamil

BTurk
Visitor II
Aug 16, 2022 11:42 PM UTC

Gneifel thank you for your support...

Sleepless nights went over with your suggestion.