Skip to main content
Associate
Nov 14, 2025 1:22 AM UTC
Question

The STM32L562E-DK cannot use STM32CubeProgrammer to download user code to flash

We encountered an issue with the STM32L562E-DK board when attempting to clear TZEN by changing the RDP level from 0 to 1 and then back to 0. Using the STM32CubeProgrammer, we can connect to the device via ST-LINK. The memory blank check indicates flash is empty, but the first byte verification fails during download. Additionally, the PC register value is 0xFFFF_FFFE, and the SP register value is 0xFFFF_FFFC.

Could you please provide guidance on resolving this issue?

5 replies

ST Technical Moderator
Nov 14, 2025 8:37 AM UTC

Hello @MelodyZ 

Try performing a regression to RDP Level 0 (option byte value 0xAA) with a full flash erase using STM32CubeProgrammer. 

If the device does not recover, boot from RSS using BOOT0 and ensure correct option bytes. 

For more details, please refer to this AN5347 in section 9 TrustZone deactivation, this may help you.

This article describes the nature of when the lock state occurs and how to best avoid and alleviate the situation.

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
MelodyZAuthor
Associate
Nov 17, 2025 7:56 AM UTC

I have set the option bytes with TZEN=0 and RDP=0, but why does the first byte still fail verification when starting from the on-chip flash?

I hope this helps with your technical support communication!

failfail

ST Technical Moderator
Nov 19, 2025 8:00 AM UTC

Hi @MelodyZ ,

Try program option bytes through JTAG/SWD and use "Hot plug" mode for option byte programming.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
MelodyZAuthor
Associate
Nov 20, 2025 3:35 AM UTC

I have used "Hot plug" to connect via JTAG/SWD, as shown in the last picture. Could you please advise which other option bytes need modification?

Thank you~

Aziz BRIGUI
ST Technical Moderator
Nov 28, 2025 9:43 AM UTC

Hello @MelodyZ

Since TZEN = 0, the address to download at is @0x08000000 not @0x0C000000, please make sure to have TrustZone disabled on your project too.

Aziz

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.