Skip to main content
Associate
Mar 16, 2026 7:04 AM UTC
Solved

TARGETSEL problem with multidrop on STM32WL and U0

I am trying to do multidrop with STM32WL5MOC and STM32U031. I have some issues:

[1] When WL5MOC is the only active MCU in the circuit (U0 is not powered on) I cannot connect M4 core using TargetSel=0x04970041 option:

  • I can connect to M0+ core using tagetsel (STM32_Programmer_CLI -c port=swd TargetSel=0x04970041 ap=1 mode=hotplug)
  • If I try the same with ap=0, CLI cannot connect to M4 core and retires with ap=1 and then connects M0+ core again
  • There is no issue when not using targetsel option and U0 is disconnected. I can connect both WL5 cores with ap=0 and ap=1 options.

[2] If I power on U0 and try multidrop, I cannot connect any of the cores of WL5:

  • I can connect U0 with targetsel option(STM32_Programmer_CLI -c port=swd TargetSel=0x04590041 ap=0 mode=hotplug).. At first CLI cannot connect with ap=0 and retries with ap=1 and then connects.
  • Interestginly If I try ap=1 directly, it cannot connect to U0 (STM32_Programmer_CLI -c port=swd TargetSel=0x04590041 ap=0 mode=hotplug)

Am I missing something?

 

Aziz BRIGUI
Aziz BRIGUIBest answer
ST Technical Moderator
May 21, 2026 12:33 PM UTC

Hi @barmagan,

Should be fixed in the next release coming by the end of June. Stay tuned and don't hesitate to confirm once tested on your side.

Aziz

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

4 replies

barmaganAuthor
Associate
Mar 16, 2026 7:37 AM UTC

Additional Info:

I am using latest sw and fw:

  • STLINK-V3PWR with firmware V4J7B3P6
  • STM32CubeProgrammer v2.22.0

Also tried mode=hotplug/ur/normal

Aziz BRIGUI
ST Technical Moderator
Mar 17, 2026 9:30 AM UTC

Hi @barmagan

This is a known limitation for STM32CubeProgrammer v2.22.0, you can find more details here: STM32CubeProgrammer errata 2.22.x - stm32mcu.

Our team is working internally for a fix. I'll let you know if there's any updates (Internal tracking number: TPRG-91).

Aziz

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
barmaganAuthor
Associate
May 21, 2026 11:03 AM UTC

Hi @Aziz BRIGUI 

Is there any progress on this subject?

 

Regards,

B.