Skip to main content
aonsquared
Associate III
Jan 15, 2020 1:31 AM UTC
Solved

SWO viewer for STM32CubeProgrammer?

Hi,

We're currently using the SWO viewer in the old ST-Link Utility in Windows.

However, this is a bit inconvenient for us because our main development is in Linux. Is SWO support planned for STM32CubeProgrammer? Even just STM32Programmer_CLI SWO support would be much appreciated.

This topic has been closed for replies.
Houda GHABRI
Houda GHABRIBest answer
ST Employee
Dec 16, 2020 9:37 AM UTC

Hi @aonsquared​ @psztoch​ ,

I come back to the this thread to announce that SWO viewer is now supported in 2.6.0 (also in 2.5.0).

Hope this helps other users using SWO.

Houda

2 replies

psztoch
Associate II
Jan 21, 2020 5:01 PM UTC

No support for SWO is very important lack in feature list!!!

It should support use of shared st-link-server.

It should support connection via TCP port using st-link_gdbserver, too.

Houda GHABRI
Houda GHABRIBest answer
ST Employee
Dec 16, 2020 9:37 AM UTC

Hi @aonsquared​ @psztoch​ ,

I come back to the this thread to announce that SWO viewer is now supported in 2.6.0 (also in 2.5.0).

Hope this helps other users using SWO.

Houda