Skip to main content
Associate II
Aug 18, 2025 9:03 AM UTC
Solved

STSPIN32G4 not detected after first programming – Boot0 not exposed

Hello,

I’m working with the STSPIN32G4. I was able to program the MCU once successfully, but since then neither STM32CubeIDE nor STM32CubeProgrammer are able to detect it anymore.

The main issue is that I did not expose the BOOT0 pin on my board, so I can’t easily force it into system bootloader mode.

Has anyone faced a similar issue?

  • Is there any workaround without physical access to the BOOT0 pin?

  • Would SWD still work if the application firmware misconfigured the debug pins?

  • Any suggestions for recovering the MCU in this situation?

I’d really appreciate any help or guidance.

Thanks in advance!

suyog1_0-1755507639815.pngsuyog1_1-1755507662285.png

suyog1_2-1755507737042.png

 

This topic has been closed for replies.
Ozone
OzoneBest answer
Principal
Aug 18, 2025 9:52 AM UTC

> The main issue is that I did not expose the BOOT0 pin on my board, so I can’t easily force it into system bootloader mode.

This is probably a lapse you make only once. But a mass erase / de-bricking through the system bootloader is very common during development.

Your firmware probably hangs in a fault handler, or has locked up due to a critical error in a default handler.
As mentioned, you will need the BOOT0 pin.
Perhaps solder a wire contraption with a removable jumper to the pin.

In theory you can try to catch the core with the debugger after power-on reset before it faults, but the probability is close to zero.

6 replies

AScha.3
Super User
Aug 18, 2025 9:42 AM UTC

Hi,

BOOT0  has to be on GND level. No workaround , if used as BOOT0 .

Otherwise try connect under reset (with hardware reset , nrst connected);

then set option bytes ...to not use BOOT0 pin as BOOT0 .

from rm STM32G4 :

AScha3_0-1755510729850.png

 

If you feel a post has answered your question, please click on " Best Answer ".
suyog1Author
Associate II
Aug 18, 2025 9:51 AM UTC

But I was able to program it using SWD once.

Ozone
OzoneBest answer
Principal
Aug 18, 2025 9:52 AM UTC

> The main issue is that I did not expose the BOOT0 pin on my board, so I can’t easily force it into system bootloader mode.

This is probably a lapse you make only once. But a mass erase / de-bricking through the system bootloader is very common during development.

Your firmware probably hangs in a fault handler, or has locked up due to a critical error in a default handler.
As mentioned, you will need the BOOT0 pin.
Perhaps solder a wire contraption with a removable jumper to the pin.

In theory you can try to catch the core with the debugger after power-on reset before it faults, but the probability is close to zero.

suyog1Author
Associate II
Aug 19, 2025 9:55 AM UTC

I have xonnected boot0 pin to gnd. Now I am able to connect to the MCU using cube programmer, but not able to program it!! Please help
I have attached the log file for reference.











Ozone
Principal
Aug 19, 2025 10:29 AM UTC

Have you tried a mass erase ?
The Cube programmer should support this.

The option byte and sector erase errors in the log file look strange, although I don't have any experience with the G431.

suyog1Author
Associate II
Aug 19, 2025 12:25 PM UTC

Now some how I connected my boot-0 pin to GND. Now stm32cube programmer is able to connect to the MCU, but not able to program it. I have attached the log file from stm32 cube programmer. I was also able to download the option bytes of the MCU.

Till now, I was able to program it once after full chip erase using cube programmer. This is very weird behaviour.

suyog1_4-1755606155234.png