Skip to main content
FRieb.1
Associate II
Nov 24, 2021 11:42 AM UTC
Question

STMCubeProgrammer - Start after programming not possible with Readout Protection Level 1

I want to start the application after programming it and setting the readout protection. But when the readout protection is set to level 1 this is no longer possible. With level 0 it works as usual.

This topic has been closed for replies.

2 replies

TDK
Nov 24, 2021 3:03 PM UTC

How specifically are you starting the application with STM32CubeProgrammer and what error message or undesired behavior do you get when it is "no longer possible"?

"If you feel a post has answered your question, please click ""Accept as Solution""."
FRieb.1
FRieb.1Author
Associate II
Nov 25, 2021 7:07 AM UTC

When I select <Run after programming> the application runs after programming if the readout protection is at level 0.

If the readout protection is at level 1 the application is not running after programming. The Log says " Application is running, Please Hold on..." and "Start operation achieved successfully" but it doesn`t work.0693W00000GYo1QQAT.png