Skip to main content
videojames
Associate III
Feb 8, 2023 5:05 AM UTC
Question

STMCube IDE: View generated run command in console

Hello,

I am troubleshooting an issue with a provisioning and testing script using the STM32_Programmer_CLI. I get "Failed to erase memory errors" in the CLI but running (as far as I can tell) the same options in CubeIDE does not generate the same error.

It would be very helpful if I could see the CLI command in full when I run or debug on CubeIDE.

Is there such a method for doing so?

Thankyou

This topic has been closed for replies.

1 reply

Javier1
Principal
Feb 13, 2023 4:40 PM UTC

you should elavorate a bit more, what about including your script for us to see?

hit me up in https://www.linkedin.com/in/javiermuñoz/