STM32WB BLE Stack 1.23.0 Not Working on STM32WB55CGU6 – Firmware Version Shows v0.0.0.0
- 2 replies
- 527 views
Describe the Setup
Device: STM32WB55CGU6
Tool: STM32CubeProgrammer
Describe the Issue
When attempting to flash the BLE stack version 1.23.0 to the STM32WB55CGU6 using STM32CubeProgrammer, I encountered issues with the following firmware files:
stm32wb5x_BLE_Stack_full_extended_fw.bin
stm32wb5x_BLE_Stack_full_fw.bin
stm32wb5x_BLE_Stack_light_fw.bin
The version information is not displayed in the “Selected File” section of STM32CubeProgrammer. After flashing, the FUS reports version v0.0.0.0, indicating that the firmware may be invalid or improperly formatted. This makes it impossible to proceed with BLE stack initialization or further development.
I would greatly appreciate any clarification on whether these binaries are compatible with the STM32WB55CGU6 and, if not, whether a corrected version of the BLE stack 1.23.0 can be provided.
Additionally, since I’m unable to downgrade the firmware on my device, I would like to kindly ask if it’s possible to release version 1.24.0 of the BLE stack ahead of schedule, as this may help resolve the issue.
Thank you for your support.