Skip to main content
Associate
Feb 4, 2026 12:29 AM UTC
Question

STM32U575/STM32U585 Programming time different

Hi Everybody,

     Now i met an issue for STM32U575/STM32U585 Programming time different, below is my test log, i don't why get the different time, since i do the erase in any time. The blank chip programming time is 34s, and NOT BLANK chip programming time is 13s.

 

NOT Blank
STM32_Programmer_CLI.exe -c port=SWD sn=55FF69064978865014230767 freq=8000 -e all -w "D:\Download_Tool\FW\EVT_SMT_2.0.1.6\RLT_ReleaseStandaloneNoAlgo_2.0.1.6.bin" 0x08000000 -v
      -------------------------------------------------------------------
                       STM32CubeProgrammer v2.14.0                  
      -------------------------------------------------------------------
 
ST-LINK SN  : 55FF69064978865014230767
ST-LINK FW  : V2J45S7
Board       : --
Voltage     : 1.86V
SWD freq    : 4000 KHz
Connect mode: Normal
Reset mode  : Software reset
Device ID   : 0x482
Revision ID : Rev W
Device name : STM32U575/STM32U585
Flash size  : 2 MBytes
Device type : MCU
Device CPU  : Cortex-M33
BL Version  : 0x93
Debug in Low Power mode enabled
Mass erase ... 
Mass erase successfully achieved
      -------------------------------------------------------------------
        Choose flashing speed for Cortex M33 series.(default speed=Reliable)                  
      -------------------------------------------------------------------
Memory Programming ...
Opening and parsing file: RLT_ReleaseStandaloneNoAlgo_2.0.1.6.bin
  File          : RLT_ReleaseStandaloneNoAlgo_2.0.1.6.bin
  Size          : 1.04 MB 
  Address       : 0x08000000 
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 133]
Download in Progress:
                                                   0%
                                    71%                100%
File download complete
Time elapsed during download operation: 00:00:13.422
Verifying ...
Read progress:
                                                   50%
                                                   100%
Download verified successfully 
 
Blank Chip:
STM32_Programmer_CLI.exe -c port=SWD sn=49FF6E067189495142410987 freq=8000 -e all -w "D:\Download_Tool\FW\EVT_SMT_2.0.1.6\RLT_ReleaseStandaloneNoAlgo_2.0.1.6.bin" 0x08000000 -v
      -------------------------------------------------------------------
                       STM32CubeProgrammer v2.14.0                  
      -------------------------------------------------------------------
 
ST-LINK SN  : 49FF6E067189495142410987
ST-LINK FW  : V2J42S7
Board       : --
Voltage     : 1.75V
SWD freq    : 4000 KHz
Connect mode: Normal
Reset mode  : Software reset
Device ID   : 0x482
Revision ID : Rev W
Device name : STM32U575/STM32U585
Flash size  : 2 MBytes
Device type : MCU
Device CPU  : Cortex-M33
BL Version  : 0x93
Debug in Low Power mode enabled
Mass erase ... 
 
Mass erase successfully achieved
      -------------------------------------------------------------------
        Choose flashing speed for Cortex M33 series.(default speed=Reliable)                  
      -------------------------------------------------------------------
Memory Programming ...
Opening and parsing file: RLT_ReleaseStandaloneNoAlgo_2.0.1.6.bin
  File          : RLT_ReleaseStandaloneNoAlgo_2.0.1.6.bin
  Size          : 1.04 MB 
  Address       : 0x08000000 
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 133]
Download in Progress:
 0%
 71% 100%
File download complete
Time elapsed during download operation: 00:00:34.281
Verifying ...
Read progress:
                                                   50%
                                                   100%
Download verified successfully 
C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\STM32_Programmer_CLI.exe

6 replies

TDK
Feb 4, 2026 2:04 AM UTC

 

They are at different voltages, and quite low. It may be expected that higher voltage will complete flash operations more quickly, although I can't find anything relevant on that for this specific chip. I don't think erased/not erased is relevant here as they both perform a full erase operation first.

> STM32CubeProgrammer v2.14.0

This version is quite old. You may want to try a newer version to see if performance is improved.

"If you feel a post has answered your question, please click ""Accept as Solution""."
YongquanAuthor
Associate
Feb 4, 2026 7:12 AM UTC

Thanks for your reply, do you know how increse the voltages. Also i have tried the latest STM32Cubeprogrammer tool, it also met the same issue.

Ozone
Principal
Feb 4, 2026 7:42 AM UTC

How do you supply the target during programming ?
The supply capabilities of the debug connector are very limited, I would recommend an external supply.
In case of a ST Nucleo or Discovery board, that would be via USB (to the onboard ST-Link).
Do you talk about a custom board here ?