Skip to main content
Ypeng.1
Visitor II
Sep 5, 2020 8:07 AM UTC
Question

STM32L562EDK board can't be connected to st linker,the keill also says cpu locked up stop target!

I am working on the stm32l562 DK Board, when I program Software into STM32L5 microcontroller internal Flash memory and Configure STM32L5 static security protections, I find that stm32l562 DK Board can not conect to the stlinker with stm32cube programmer.at the same time the keil says cpu locked up ,stop target.

if I want to connect to the stlinker,what I can do?

stm32l562 DK Board

stm32cube programmer and keil

thanks

This topic has been closed for replies.

1 reply

Houda GHABRI
ST Employee
Oct 30, 2020 12:59 PM UTC

Hi @Ypeng.1​ ,

Sorry for the delay.

Can you try to connect the board in hot plug mode and tell me if it's ok?

regards,

Houda