Skip to main content
Ben K
Senior III
Nov 14, 2026 8:24 PM UTC
Question

STM32L4 devices boot to system memory after flashing with v2.23.0

Using an STM32L432KC Nucleo, I observed that STM32CubeProgrammer v2.23.0 toggles FLASH_SR.PEMPTY when it flashes an image of an odd number of 2 KiB pages to the L432KC. The board then boots into the ROM bootloader instead of the present application in flash. (I used the programmer through zephyr’s west flash on Ubuntu.)

 

Edit: duplicate of