Skip to main content
RNevi.1
Associate
Jul 11, 2022 12:44 PM UTC
Question

Stm32h750B-dk XIP STM32CubeIDE functioning examples ?

I've tried importing the examples into the IDE , complies fine but will not upload

- i get the "Failed to execute MI command:" error

if i use the stm32CubeProgrammer i can write to Flash(boot loader &program) but it never hands off to Qspi 0x90000000

i can make a small blinky program work out of the small boot flash -

so is it me ? the IDE ? a bad dev board?

(had successful projects utilizing f411' using the IDE )

possibly an explanation step by step like i'm 5years old ;) ?

This topic has been closed for replies.

2 replies

ST Technical Moderator
Jul 13, 2022 10:31 AM UTC

Hello @RNevi.1​ and welcome to the Community :),

It would be better to activate the gdb server log in your debug configuration (Debugger tab) and share it, this will help us to have more idea about the fails.

Make sure that you are using latest release of CubeIDE, Cubeprogrammer.

Try erasing the flash using Stm32Cubeporgrammer, this may solve your problem.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
RNevi.1
RNevi.1Author
Associate
Jul 14, 2022 12:18 AM UTC

log file attached

yes / latest versions of the sw

& same error after full chip erase