Skip to main content
ksale.1
Senior II
Feb 7, 2026 4:32 PM UTC
Question

STM32H750B-DK Lockup After External Flash ProgrammingSeeking Recovery Advice

  • I've been trying to run code from the external QSPI flash (MT25TL01G) and have gone through an extensive debugging process that ended with a hard lockup. Below is a detailed log of my steps.

1. Initial Setup & Goal

  • Board: STM32H750B-DK (MB1381-H750XB-B01, Product ID DK32H750B$AT1)

  • Tools: STM32CubeIDE, STM32CubeMX (FW_H7 V1.12.1), STM32CubeProgrammer.

  • Goal: Configure and debug an application to run from external QSPI flash at 0x90000000.

. Initial Setup & Goal

  • Board: STM32H750B-DK (MB1381-H750XB-B01, Product ID DK32H750B$AT1)

  • Tools: STM32CubeIDE, STM32CubeMX (FW_H7 V1.12.1), STM32CubeProgrammer.

  • Goal: Configure and debug an application to run from external QSPI flash at 0x90000000.

2. Step-by-Step Troubleshooting & Results

A. CubeMX & Project Configuration

  • Created project via Board Selector (not MCU selector).

  • Verified QUADSPI configured in Memory-Mapped mode (Clock Prescaler=2, CS High Time=2, Flash Size=26).

Programming & External Loader

  • STM32CubeProgrammer: Successfully programmed my .hex file to 0x90000000 (log confirms full erase, download, and verify).

  • External Loader: MT25TL01G_STM32H750B-DISCO.stldr is selected with both Enabled and Initialize checked in the IDE debug configuration.

C. Debugging Attempts & Failures

  • Default debug launch always halted at 0x80011b0 (internal flash), ignoring external flash.

  • Attempt 1 (VTOR): Added SCB->VTOR = 0x90000000; early in main() and also tried setting it via GDB Run Commands (set *((unsigned int *)0xE000ED08) = 0x90000000).

  • Result: The debugger seemed to jump but immediately hit a HardFault or Lockup state. The processor appears to crash as soon as it tries to fetch instructions from external flash.

  • Attempt 2 (Run from CubeProgrammer): Used CubeProgrammer's "Run after programming" feature. The board enters a locked state (no functional code execution, debugger reports "ARM M in lockup state").

Current Status & Questions

The board is now unresponsive in normal operation. The core seems to be in a lockup, likely because it is trying to boot from/branch to an uninitialized or incorrectly accessed QSPI memory region.

My specific questions for the community are:

  1. Recovery: What is the most reliable way to recover from this lockup on the STM32H750B-DK? I understand I may need to force boot from internal memory, but the board lacks a standard BOOT0 jumper. Should I bridge a specific resistor pad (e.g., R100)? Or is a full chip erase via STM32CubeProgrammer under reset sufficient?

  2. Root Cause: Given that the flash programs and verifies correctly, what step am I missing to ensure the QSPI is initialized for memory-mapped mode before the CPU attempts to execute from 0x90000000? Does the SystemInit() function need modification for this board?

  3. Configuration: Has anyone successfully automated this process with this specific board? What is the correct sequence in CubeMX/IDE to ensure the application is built and debugged for external flash from the start?