Skip to main content
YNam.1
Visitor II
Aug 12, 2022 11:51 AM UTC
Solved

STM32H750 externalloader fails on SystemClock_Config.

Hi.

I'm developing with custom board which has a custom QSPI (EN25QX128A - 16Mbytes flash), so I need to make an external loader used by STM32CubeProgrammer.

First I wrote a code that interacts with QSPI and it works fine.

So I changed this code to fullfill the external loader specification.

  • Init() as an entry point
  • Linker configuration
  • No diagnostics on unused functions

But when I connect the target board by clicking "Connect" in STM32CubeProgrammer, I checked that "Init()" is called but SystemClock_Cofnig() fails.

I tried to change clock-setting in various ways, but still get stuck in Error_Handler.

What am I missing working with External loader?

Please help me to get out of this trap.

Thanks.

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Aug 12, 2022 12:38 PM UTC

Perhaps that the clock / pll is already running?

​

​Check the local/auto variable is cleared.

USART cam be used for diagnostic output.

System can run from HSI​.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

1 reply

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Aug 12, 2022 12:38 PM UTC

Perhaps that the clock / pll is already running?

​

​Check the local/auto variable is cleared.

USART cam be used for diagnostic output.

System can run from HSI​.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..