Skip to main content
Visitor II
Feb 26, 2024 3:11 PM UTC
Solved

STM32G4 bootloader via canbus

Im trying to bootloader my firmware in my nucleo G431RB vía canbus with a StLink v3 set,  its posible?.

 In An2606 says there is no opción.

Do i have to write the bootloader ? And with that i will be able to load vía StLink v3 set?

  

This topic has been closed for replies.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
Feb 26, 2024 4:29 PM UTC

Hello @PedroLuis and welcome to the ST Community :smiling_face_with_smiling_eyes:.

For the STM32G431RB, the only hardware ressources that can be available are USART, SPI, DFU and I2C. CAN is not available for bootloader. Look at the AN2606 and the product datasheet.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

7 replies

STTwo-32
STTwo-32Best answer
ST Technical Moderator
Feb 26, 2024 4:29 PM UTC

Hello @PedroLuis and welcome to the ST Community :smiling_face_with_smiling_eyes:.

For the STM32G431RB, the only hardware ressources that can be available are USART, SPI, DFU and I2C. CAN is not available for bootloader. Look at the AN2606 and the product datasheet.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate
May 6, 2024 6:29 AM UTC

Is it possible if I write the bootloader vía canbus by myself? 

STTwo-32
ST Technical Moderator
May 6, 2024 6:51 AM UTC

Hi 

Bootloader is not possible Via CAN in the STM32G431RB.

Best Reagrds.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
mƎALLEm
ST Technical Moderator
Feb 26, 2024 4:40 PM UTC

Hello,

Indeed no bootloader over CAN bus. See AN2606 / Table 99. STM32G431xx/441xx configuration in system memory boot mode.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
tdecker2
Associate II
Aug 8, 2024 9:23 AM UTC

Yes, the integrated bootloader maybe does not support the CAN interface. But sure a custom bootloader can use whatever interface is available in the controller to receive a new firmware.

I didn't use it yet, but have a look at the OpenBLT bootloader which supports CAN and the G4 family. https://www.feaser.com/openblt

 

Associate
Aug 8, 2024 9:32 AM UTC

As I thought, have looked at OpenBLT but as it is for a commercial (proprietary) product we need a commercial license for it so looking at how hard building our own would be with Open bootloader.