Skip to main content
Associate
Jun 25, 2025 12:40 PM UTC
Question

STM32G071CBT6TR Bootloader Upload Fails After First Flash

I am contacting you to report and request assistance with a recurring issue I am facing while working with the STM32G071CBT6TR microcontroller. I am experiencing problems with the bootloader during UART-based firmware uploads.

The microcontroller programs successfully only the first time via UART using a USB-to-Serial converter (FT232RL). However, after a successful first upload, subsequent upload attempts fail, even though nothing changes in the hardware or the code.


Technical Setup:

  • MCU: STM32G071CBT6TR

  • Programming Method: UART (USART1) using USB-to-Serial (FT232RL)

  • Baud Rate: 115200

  • Parity: Even (as required by STM32 bootloader)

  • Boot Mode Configuration:

    • BOOT0 is connected to 3.3V

    • Reset pin is manually triggered before upload

  • Software: STM32CubeProgrammer

  • Port Status: COM port opens successfully


the observed behavior: 

  1. First Upload:
    Upload works perfectly with the default settings using STM32CubeProgrammer over UART.

  2. Following Uploads:
    All subsequent attempts fail with the following error:

    CopyEdit
    Timeout error occurred while waiting for acknowledgement. Error: Activating device: KO. Please verify the boot mode configuration and check the serial port configuration.

    Despite confirming that BOOT0 is still high, the reset pin is pressed, and all connections remain unchanged, the bootloader fails to respond.

  3. Serial Output Behavior:

    • With parity set to even: readable output appears, but the upload still fails.


i've tried the following : 

  • Verified all connections (TX/RX orientation, BOOT0 high, proper reset sequence).

  • Tried different USB-to-Serial adapters.

  • Checked signal integrity and power stability (3.3V regulated).

  • Tried slower baud rates and different computers.

  • Attempted to enter bootloader manually again via BOOT0 + Reset combo, to no avail.

I would greatly appreciate your assistance in diagnosing and resolving this issue. Specifically, I would like to know:

  1. Is this a known issue with the STM32G071CBT6TR UART bootloader?

  2. Are there any documented limitations or special procedures required after the first flash?

  3. Is there a way to fully reset the bootloader to an initial working state?


Please let me know if you need schematics, logic analyzer captures, or any additional diagnostic information.

Thank you in advance for your time and support.

Best regards,

This topic has been closed for replies.

4 replies

TDK
Jun 25, 2025 1:01 PM UTC

The BOOT0 pin state is ignored on this microcontroller by default. You need to change the option bytes if you want different behavior.

On the first boot, since flash is empty, it boots into the bootloader. After that, it boots into user flash.

 

To recover, you will need to change the option bytes using a SWD programming connection.

"If you feel a post has answered your question, please click ""Accept as Solution""."
adem1Author
Associate
Jun 25, 2025 1:15 PM UTC

i have some other question if you mind

1) Is modifying the option bytes via SWD the only method to enable bootloader mode using BOOT0 on this MCU?

2) Is there any documentation or official application note that clearly describes this boot behavior for the STM32G071 series?

3) Is there a recommended way to safely configure option bytes so the bootloader is always available when BOOT0 is high?

 

 

TDK
Jun 25, 2025 1:48 PM UTC

1) After it's already programmed, yes. If not yet programmed, the bootloader could do this via STM32CubeProgrammer.

2) AN2606 describes how to get into the bootloader. The reference manual describes default option bytes.

3) Set BOOT_SEL = 0 to have the BOOT0 pin be sampled on startup rather than the nBOOT0 bit.

TDK_0-1750859211758.png

 

"If you feel a post has answered your question, please click ""Accept as Solution""."