Skip to main content
HPuij.1
Visitor II
Jan 10, 2023 1:46 PM UTC
Solved

STM32G030 Missing option byte NRST_MODE with STM32CubeProgrammer CLI

I am trying to modify the NRST_MODE option byte for a STM32G030 MCU.

I have changed the reset pin to GPIO using the GUI, but that is not very usefull for a production environment.

The option byte in not available from the CLI. -> Please make it available (very usefull for production programming)

On the GUI the option is hidden away in the Registers - BETA page -> FLASH

0693W00000Y7r0mQAB.pngPlease make it available on the option bytes page for the STM32G030

For the STM32G031 it is there in the Option Bytes -> please make it also available for the STM32G030. Also the CLI has the NRST_MODE as an option byte0693W00000Y7r0OQAR.pngBeste regards, Hans.

This topic has been closed for replies.
gbm
gbmBest answer
Super User
Jan 10, 2023 2:32 PM UTC

AFAIK, G030 *officially* does not support turning off the NRST function - check the Reference Manual. Unofficialy, it's the same as G031. I have no idea why ST decided to "grey out" this functionality from G030, I suspect someone decided to "undocument" some features of G030 to make it appear to be different from G031 . The NRST in G030 may be turned off by the old good ST-Link utility, at least until ST decides to update (=spoil) it.

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice

2 replies

gbm
gbmBest answer
Super User
Jan 10, 2023 2:32 PM UTC

AFAIK, G030 *officially* does not support turning off the NRST function - check the Reference Manual. Unofficialy, it's the same as G031. I have no idea why ST decided to "grey out" this functionality from G030, I suspect someone decided to "undocument" some features of G030 to make it appear to be different from G031 . The NRST in G030 may be turned off by the old good ST-Link utility, at least until ST decides to update (=spoil) it.

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice
CTapp.1
Senior III
May 7, 2024 11:07 AM UTC

These options are missing for me using for the STM32G031.

All posts are made in a personal capacity. MISRA C++ Chair, MISRA C WG Member, Director The MISRA Consortium Limited (TMCL)