Skip to main content
DShub.1
Associate
Oct 15, 2020 11:43 AM UTC
Question

STM32F769I-DISCO, MB1225 B-02, A201800875

Hi,

I have another problem with the board "STM32F769I-DISCO, MB1225 B-02, A201800875".

I wanted to restore the original firmware of the board.

Download from ST site the image "10_2020\32F769IDISCOVERY_demo\Binary\STM32769I-DISCO_DEMO_V1.0.0_FULL.hex". Loaded it according to the "32F769IDISCOVERY_demo\readme.txt" file. I used two applications for loading:

1)STM32 ST-LINK Utility 4.6

2)STM32CubeProgrammer 2.4.0

with the same result, load the main picture with ST logo and stops. Nothing else. I think the reason is the wrong firmware revision. Before deleting the original " FW" I checked System Info and their FirmWare revision is 1.2, but I didn't find anywhere on ST site firmware such revision.

But when I do the same on the previous board 

" Board: STM32F769I-DISCO, MB1225 B-02, A192400285

 Screen : MB1166 A-02, A192400688"

with the 

"10_2020\32F769IDISCOVERY_demo\Binary\STM32769I-DISCO_DEMO_V1.0.0_FULL.hex". Loaded it according to the "32F769IDISCOVERY_demo\readme.txt" file. with STM32CubeProgrammer 2.4.0 all is working as expected.

So many problems with the board with the latest revision, with which we worked a lot normally in the past.

And the main problem is that the touchscreen does not work in our program (the separate case was opened).

Please help us to resolve it.

Best regards,

Dmitry

This topic has been closed for replies.

5 replies

Tesla DeLorean
Guru
Oct 15, 2020 12:01 PM UTC
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Associate
Oct 17, 2023 9:55 AM UTC

Hello,

I do have the exact same problem. I want to be able to restore the firmware of my STM32F769I-DISCO in version V1.2.0 as stated in the original board´s firmware system Information page but could not find the firmware image.

Unfortunatedly your link above does not work anymore.

Can you please point me to a new source?

Thank you!

Sara BEN HADJ YAHYA
ST Technical Moderator
Oct 17, 2023 2:11 PM UTC

Hello @JakeW ,

The binary demonstration files for STM32F769I-DISCO are available under Tools & Software/Compiled demos section.

SaraBENHADJYAHYA_0-1697551823609.png
SaraBENHADJYAHYA_1-1697551852601.png

Sara.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.