Skip to main content
Associate
Dec 12, 2024 7:08 PM UTC
Question

STM32F4 fails to verify after programming with STM32_Programmer_CLI over USB

I have manually verified the FLASH bytes are correct after programming, but the -v option results in "Error: Data mismatch found at address 0x10000000 (byte = 0x21 instead of 0x00)" and the process stops.

Isn't 0x10000000 a CCM address and why is it being tested and failing?  See terminal output below:

 

"C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\STM32_Programmer_CLI.exe" -c port=USB1 -d "fw.hex" -v -g 0x08000000
-------------------------------------------------------------------
STM32CubeProgrammer v2.18.0
-------------------------------------------------------------------

 

USB speed : High Speed (480MBit/s)
Manuf. ID : STMicroelectronics
Product ID : DFU in HS Mode
SN : 000000
DFU protocol: 1.1
Board : --
IAP
Opening and parsing file: fw.hex


Memory Programming ...
File : fw.hex
Size : 459.21 KB
Address : 0x080A0000


Erasing memory corresponding to segment 0:
Erasing memory corresponding to segment 1:
Download in Progress:
██████████████████████████████████████████████████ 100%██████████████████████████████████████

File download complete
Time elapsed during download operation: 00:00:28.989

 

Verifying ...


Read progress:
██████████████████████████████████████████████████ 100%

Error: Data mismatch found at address 0x10000000 (byte = 0x21 instead of 0x00)


Error: Download verification failed

 

This topic has been closed for replies.

1 reply

scottroAuthor
Associate
Dec 12, 2024 10:54 PM UTC

Tracked the issue down to the HEX file including bytes to initialize CCM memory as "segment 1".

The ST code must be using CCM for scratch space...

 

Resolved.