Skip to main content
RoLie
Associate
Mar 30, 2023 10:22 AM UTC
Question

STM32F105 core is halted after programming via STM32_Programmer_CLI

I need to flash a bin file on STM32F105 MCU. To do so, I use a ST-Link V3 SET connected threw ARM20-10 Pin Adapter to Tag-Connect 2050. I send this command to STM32_Programmer_CLI.exe:

C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin>STM32_Programmer_CLI.exe -c port=SWD -rdu -w "C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\Software_For_Target\program.bin" 0x08000000 -v -hardRst

It workes fine, but the MCU doesn't run after programming. When I send:

STM32_Programmer_CLI.exe -c port=SWD -score

I get "Core is halted".

To get the MCU up running, I need to disconnect and reconnect the power supply of the target. Is there any way to avoid that?

This topic has been closed for replies.