Skip to main content
Associate
Aug 16, 2025 3:32 PM UTC
Question

STM32F103C8T6 always shows “SLEEP” in CubeProgrammer, cannot perform full chip erase—no user code loaded

Hi everyone,
I'm working with an STM32F103C8T6. Even though I haven't programmed any code onto it myself, when I connect with STM32CubeProgrammer, the Registers panel immediately shows “SLEEP” (while on other ST boards it would show “HALTED”). Because of this, I can't perform a Full Chip Erase — the option appears but doesn't work.

Here’s what I’ve tried:

  • Connected only SWDIO, SWCLK, GND, and 3.3 V (no NRST).

  • CubeProgrammer shows “SLEEP,” and erase fails.

  • On other boards, “Connect under reset” works fine and allows erasing.

Possible issues I suspect:

  • No NRST pin connection → ST-Link can’t halt the MCU before it runs.

  • Option Bytes might have RDP (Read-Out Protection) enabled.

  • BOOT0 pin wrongly tied (stuck in System Memory mode).

  • Some factory test code or previous user code (making MCU go to sleep on reset).

What I tried from forum suggestions:

  • Tried “Connect under reset” with NRST — this works on other boards but seems not to work here yet.

Any ideas how to force-erase or regain access?
I’d appreciate any advice—including Option Bytes configuration, hardware wiring, or CubeProgrammer settings.
Thanks!

This topic has been closed for replies.

6 replies

AScha.3
Super User
Aug 17, 2025 8:31 PM UTC

Hi,

What st-link you use?

And set connect; software reset, and enable low power modes.

Try to connect, then show, what Cube programmer shows, screen shot.

 

If you feel a post has answered your question, please click on " Best Answer ".
Melih--Author
Associate
Aug 18, 2025 7:19 AM UTC

ı use stm32f446re nucleo board as stlink,ı can not connect stmf103 with cubeide ,only with cubeprogrammer in hot plug mode,

Melih_0-1755501452974.jpeg

this is the screenshoot ,only see stm in sleep mode , ı try my nucleo board and ı see halted,is there any chance my stm32f103c8t6 is clone 

AScha.3
Super User
Aug 18, 2025 8:52 AM UTC

>is there any chance my stm32f103c8t6 is clone 

Everything could be a "clone" , but it is very unlikely , as cpu ID (and revision) show same, as on a F103 here:

 

AScha3_0-1755506629024.png

So connect with :  software reset, nrst not needed;

Then look in OptionBytes:   rdp not set:

AScha3_1-1755506848932.png

next see  in OptionBytes: all (!) sectors have write protection OFF (= checked).

AScha3_2-1755506912884.png

down to 31:

AScha3_3-1755507059174.png

Then full/mass erase should work:

AScha3_4-1755507156378.png

Try.

 

If you feel a post has answered your question, please click on " Best Answer ".
Tesla DeLorean
Guru
Aug 17, 2025 10:15 PM UTC

Connect Under Reset from the debug pod expects NRST to be connected to the Target MCU

You can use the BOOTx pins to cause a power-up / reset into System Memory rather than a user program in FLASH sleeping the device or otherwise breaking the debug interface.

Consider have a delaying loop in System Reset to allow debugger time to connect initially

 

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..