Skip to main content
Associate
Jan 13, 2025 6:48 PM UTC
Question

STM32F070F6 bootloader

STM32 cube programmer doesn't recognize my custom board neither via USB DFU nor USART.

My circuit is simply the STM32F070F6, a 12 MHz crystal and some LEDs to control (also caps and res as necessary).

Even with boot0 direct in high or low, I'm not able to make the SW identify the MCU.

This topic has been closed for replies.

3 replies

KnarfB
Super User
Jan 13, 2025 7:26 PM UTC

look for differences compared to Getting started with STM32F0x1/x2/x8 hardware development

hth

KnarfB

Tesla DeLorean
Guru
Jan 13, 2025 8:11 PM UTC

So it sounds like your design isn't viable. Provide an actionable schematic or wiring diagram for those of us not familiar with the specifics of your design..

Make sure all the power pins, including VDDA/VSSA are connected, even if your aren't using ADC/DAC, the reset circuit is in that domain.

Check part orientation. Check pin numbering

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
EdDnAuthor
Associate
Jan 14, 2025 11:01 AM UTC

The circuit is as follow.
3V3 is regulated from a 5V source.