Skip to main content
AAmer.1
Associate II
May 18, 2020 3:29 PM UTC
Question

STM32CubeProgrammer-Windows OS

Hello,

DFU is not working in STM32Cube Programmer, I can see the connected board in device manager under universal serial bus controllers, please your advise.

Thanks

This topic has been closed for replies.

11 replies

TDK
May 18, 2020 8:33 PM UTC

Does it show up in device manager as a DFU device? Show a screenshot. It's not in that mode by default, you need to start the bootloader with USB enabled and nothing else talking to the chip.

"If you feel a post has answered your question, please click ""Accept as Solution""."
AAmer.1
AAmer.1Author
Associate II
May 19, 2020 2:40 PM UTC

No it appears as USB serial converter

Nesrine.JLASSI
Visitor II
May 18, 2020 8:39 PM UTC

Hello @AAmer.1​ 

which board do you use ?

Best regards,

Nesrine

AAmer.1
AAmer.1Author
Associate II
May 19, 2020 9:42 AM UTC

Hello Nesrine,

I have our own board.

BR

Nesrine.JLASSI
Visitor II
May 19, 2020 9:59 AM UTC

Hello @AAmer.1​ 

So, it is necessary to know if your Board contains a bootloader or not.

Best regards,

Nesrine

AAmer.1
AAmer.1Author
Associate II
May 19, 2020 10:03 AM UTC

this is the reason why I'm trying to connect to it, I need to flash it with bootloader.

Nesrine.JLASSI
Visitor II
May 19, 2020 10:04 AM UTC

It is necessary to check the boot on the system memory.

AAmer.1
AAmer.1Author
Associate II
May 19, 2020 10:09 AM UTC

yes I knew, the boot are correct, strange.

Nesrine.JLASSI
Visitor II
May 19, 2020 2:47 PM UTC

Hello @AAmer.1​ 

I think that the problem is on the user's own board not on the Cubeprogrammer.

Best regards,

Nesrine

Olivier GALLIEN
ST Technical Moderator
May 20, 2020 6:11 AM UTC

Hi @AAmer.1​ 

This is not clear here if we are talking about a tool problem ( STM32CubeProgrammer/ Windows) or a board bring-up problem ( you use your own board ?)

So did you already succeed to use STM32CubeProgrammer on one ST devkit such as DK2 or EV1 ?

Please confirm by "own board" you are talking about a custom PCB design at your end ? Which STM32MP1 reference ?

Is your design close to ST board ?

Thanks for answer.

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
PatrickF
ST Employee
May 20, 2020 6:44 AM UTC
In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent