Skip to main content
Associate III
Aug 6, 2026 9:38 PM UTC
Question

STM32CubeProgrammer V2.21.0 update failure

STM32CubeProgrammer V2.21.0 displays an update avaliable icon and when I click it it offers to update to V2.23.0, but when I let it try to update it appears to download something then some windows flash up for a moment then STM32CubeProgrammer restarts but is still V2.21.0.

I am on Windows 11

4 replies

Aziz BRIGUI
ST Technical Moderator
Aug 20, 2026 1:11 PM UTC

Hi ​@SamMiddleton,

What proxy option are you using ?

Aziz

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Associate III
Aug 20, 2026 9:18 PM UTC

How do I find that out?

Karl Yamashita
Super User
Aug 20, 2026 11:55 PM UTC

using the question mark in the bottom left corner of CubeProgrammer

 

 

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source