Skip to main content
Visitor II
Feb 17, 2025 9:38 PM UTC
Solved

STM32CubeProgrammer v2.18.0 - missing DBANK/DUALBANK option bytes when cli is called

Hello,

Its just simple, when STM32_Programmer_CLI -c port=SWD mode=HotPlug -ob displ command is called - "Bit 21 DUALBANK: Dual-bank configuration" missing in report.

stdout:

 

 

 

-------------------------------------------------------------------
 STM32CubeProgrammer v2.18.0 
 -------------------------------------------------------------------
ST-LINK SN : 
ST-LINK FW : V3J15M7B5S1
Board : STLINK-V3SET
Voltage : 3.27V
SWD freq : 8000 KHz
Connect mode: Hot Plug
Reset mode : Software reset
Device ID : 0x482
Revision ID : Rev W
Device name : STM32U575/STM32U585
Flash size : 2 MBytes
Device type : MCU
Device CPU : Cortex-M33
BL Version : 0x93
Debug in Low Power mode enabled
UPLOADING OPTION BYTES DATA ...
 Bank : 0x00
 Address : 0x40022040
 Size : 48 Bytes
 0%
 100%
OPTION BYTES BANK: 0
 Read Out Protection:
 RDP : 0xAA (Level 0, no protection) 
 BOR Level:
 BOR_LEV : 0x0 (BOR Level 0, reset level threshold is around 1.7 V) 
 User Configuration:
 TZEN : 0x0 (Global TrustZone security disabled) 
 nRST_STOP : 0x1 (No reset generated when entering Stop mode) 
 nRST_STDBY : 0x1 (No reset generated when entering Standby mode) 
 nRST_SHDW : 0x1 (No reset generated when entering the Shutdown mode) 
 SRAM134_RST : 0x1 (SRAM1, SRAM3 and SRAM4 not erased when a system reset occurs) 
 IWDG_SW : 0x1 (Software independent watchdog) 
 IWDG_STOP : 0x1 (IWDG counter active in stop mode) 
 IWDG_STDBY : 0x1 (IWDG counter active in standby mode) 
 WWDG_SW : 0x1 (Software window watchdog) 
 SWAP_BANK : 0x0 (Bank 1 and bank 2 address are not swapped) 
 BKPRAM_ECC : 0x1 (Backup RAM ECC check disabled) 
 SRAM3_ECC : 0x1 (SRAM3 ECC check disabled) 
 SRAM2_ECC : 0x1 (SRAM2 ECC check disabled) 
 SRAM2_RST : 0x1 (SRAM2 is not erased when a system reset occurs) 
 nSWBOOT0 : 0x1 (BOOT0 taken from PH3/BOOT0 pin) 
 nBOOT0 : 0x1 (nBOOT0 = 1) 
 PA15_PUPEN : 0x1 (USB power delivery dead-battery disabled/ TDI pull-up activated) 
 IO_VDD_HSLV : 0x0 (High-speed IO at low VDD voltage feature disabled (VDD can exceed 2.5 V)) 
 IO_VDDIO2_HSLV: 0x0 (High-speed IO at low VDDIO2 voltage feature disabled (VDDIO2 can exceed 2.5 V)) 
 Boot Configuration:
 NSBOOTADD0 : 0x100000 (0x8000000) 
 NSBOOTADD1 : 0x17F200 (0xBF90000) 
 Write Protection 1:
 WRP1A_PSTRT : 0x7F (0x80FE000) 
 WRP1A_PEND : 0x0 (0x8000000) 
 UNLOCK_1A : 0x1 (WRP1A start and end pages unlocked) 
 WRP1B_PSTRT : 0x7F (0x80FE000) 
 WRP1B_PEND : 0x0 (0x8000000) 
 UNLOCK_1B : 0x1 (WRP1B start and end pages unlocked) 
 Write Protection 2:
 WRP2A_PSTRT : 0x7F (0x81FE000) 
 WRP2A_PEND : 0x0 (0x8100000) 
 UNLOCK_2A : 0x1 (WRP2A start and end pages unlocked) 
 WRP2B_PSTRT : 0x7F (0x81FE000) 
 WRP2B_PEND : 0x0 (0x8100000) 
 UNLOCK_2B : 0x1 (WRP2B start and end pages unlocked) 

 

 

 

 

 

 

This topic has been closed for replies.
Maryem
MaryemBest answer
ST Employee
Feb 27, 2025 9:34 AM UTC

Hello @MarekK ,

 

For high flash sizes, the DBANK bit is always set to 1, so it was decided to remove it from the Option Bytes tab since it is not configurable. For lower flash sizes, the DBANK bit remains visible and configurable.
Please refer to Table 52 of the RM0456 for more details.

 

Maryem.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

3 replies

STTwo-32
ST Technical Moderator
Feb 17, 2025 11:10 PM UTC

Hello @MarekK and welcome to the ST Community.

It seems to be missing on my side too. I've escalated to the concerned team for correction on the future (under internal ticket number 203898).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Maryem
MaryemBest answer
ST Employee
Feb 27, 2025 9:34 AM UTC

Hello @MarekK ,

 

For high flash sizes, the DBANK bit is always set to 1, so it was decided to remove it from the Option Bytes tab since it is not configurable. For lower flash sizes, the DBANK bit remains visible and configurable.
Please refer to Table 52 of the RM0456 for more details.

 

Maryem.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Associate
Sep 24, 2025 9:49 AM UTC

Hello,

I'm using the STM32U545VET6, which has 512 KB of flash. In STM32CubeProgrammer 2.20.0, there is no DBANK or DUALBANK in option byte in the user configuration. Was this intentionally removed, or is it a bug?

Additionally, this is for a TF-M configuration on this chip. Will there be any issues if this bit is not set?

Best,

Lezhi