Skip to main content
KKhan.4
Associate II
Mar 21, 2023 3:41 AM UTC
Question

STM32CubeProgrammer using 0x40022020 to access Option Bytes of STM32G0

I am using STM32CubeProgrammer to access Option bytes of stm32g070kbt6. Everything is okay but I don't understand by STM32CubeProgrammer is using 0x40022020 to get option bytes when the documentation says it should be between 0x1FFF 7800 - 0x1FFF 787F.

PS C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin> ./STM32_Programmer_CLI -c port=swd -ob displ
 
 -------------------------------------------------------------------
 
 STM32CubeProgrammer v2.12.0
 
 -------------------------------------------------------------------
 
 
 
ST-LINK SN : 31FF74064D4E353830240243
 
ST-LINK FW : V2J40S7
 
Board : --
 
Voltage : 3.24V
 
SWD freq : 4000 KHz
 
Connect mode: Normal
 
Reset mode : Software reset
 
Device ID : 0x460
 
Revision ID : Rev B
 
Device name : STM32G07x/STM32G08x
 
Flash size : 128 KBytes
 
Device type : MCU
 
Device CPU : Cortex-M0+
 
BL Version : 0xB2
 
Debug in Low Power mode enabled
 
 
 
 
 
UPLOADING OPTION BYTES DATA ...
 
 
 
 Bank : 0x00
 
 Address : 0x40022020
 
 Size : 112 Bytes
 
 
 
██████████████████████████████████████████████████ 100%
 
 
 
 
 
OPTION BYTES BANK: 0
 
 
 
 Read Out Protection:
 
 
 
 RDP : 0xAA (Level 0, no protection)
 
 
 
 BOR Level:
 
 
 
 BOR_EN : 0x1 (Configurable brown out reset enabled, values of BORR_LEV and BORF_LEV taken into account)
 
 BORR_LEV : 0x0 (BOR rising level 1 with threshold around 2.1 V)
 
 BORF_LEV : 0x0 (BOR falling level 1 with threshold around 2.0 V)
 
 
 
 User Configuration:
 
 
 
 nRST_STOP : 0x1 (No reset generated when entering Stop mode)
 
 nRST_STDBY : 0x1 (No reset generated when entering Standby mode)
 
 nRST_SHDW : 0x1 (No reset generated when entering the Shutdown mode)
 
 IWDG_SW : 0x1 (Software independant watchdog)
 
 IWDG_STOP : 0x1 (IWDG counter active in stop mode)
 
 IWDG_STDBY : 0x1 (IWDG counter active in standby mode)
 
 WWDG_SW : 0x1 (Software window watchdog)
 
 RAM_PARITY_CHECK: 0x1 (SRAM parity check disable)
 
 nBOOT_SEL : 0x1 (BOOT0 signal is defined by nBOOT0 option bit)
 
 nBOOT1 : 0x1 (Boot from Flash if BOOT0 = 0, otherwise system memory)
 
 nBOOT0 : 0x1 (nBOOT0=1)
 
 NRST_MODE : 0x3 (Bidirectional reset: NRST pin configured in reset input/output mode (legacy mode))
 
 IRHEN : 0x0 (Internal resets are propagated as simple pulse on NRST pin)
 
 
 
 PCROP Protection:
 
 
 
 PCROP1A_STRT : 0xFF (0x801FE00)
 
 PCROP1A_END : 0x0 (0x8000200)
 
 PCROP_RDP : 0x0 (PCROP zone is kept when RDP is decreased)
 
 PCROP1B_STRT : 0xFF (0x801FE00)
 
 PCROP1B_END : 0x0 (0x8000200)
 
 
 
 Write Protection:
 
 
 
 WRP1A_STRT : 0x3F (0x801F800)
 
 WRP1A_END : 0x0 (0x8000000)
 
 WRP1B_STRT : 0x3F (0x801F800)
 
 WRP1B_END : 0x0 (0x8000000)
 
 
 
 FLASH security:
 
 
 
 BOOT_LOCK : 0x0 (Boot based on the pad/option bit configuration)
 
 SEC_SIZE : 0x0 (0x8000000)

This topic has been closed for replies.

1 reply

Peter BENSCH
ST Technical Moderator
Mar 21, 2023 7:49 PM UTC

This seems a bit confusing, but you will find an explanation in the respective reference manual, section 3.4.2 FLASH option byte programming:

Upon system reset, the option bytes are copied into the following option registers that can be read and written by software:

  • FLASH_OPTR
  • [...]

These registers are also used to modify options. If these registers are not modified by user, they reflect the options states of the system.

The omission character [...] stands for additional registers that are different between STM32G0x0 (RM0454) and STM32G0x1 (RM0444).

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.